STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DCMI format support

Posted on July 02, 2015 at 14:10HelloAccording to DCMI section of stm32f407 datasheet and RM0090, RGB565 is supported.Is raw RGB(888) supported too?Thanks.

Can you help me about getting good picture in the STM32

Posted on August 27, 2013 at 11:23I can get this Picture.But I don't know how I can correct this mistake! My code:/* DCMI configuration *******************************************************/   DCMI_InitStructure.DCMI_CaptureMode = DCMI_CaptureMo...

0690X000006050ZQAQ.png
muhammet by Associate II
  • 1635 Views
  • 3 replies
  • 0 kudos

USB HID stop working

Posted on July 01, 2015 at 09:42Hi,We are working on USB HID with 64bytes IN and OUT reports with a stm32f401. We're using the stm32cude v1.6.0 for generated code, and we developped on KEIL v5.The USB peripheral working well, we can speak with it fr...

ambroise by Associate II
  • 2445 Views
  • 4 replies
  • 0 kudos

matlab problem with virtual com port

Posted on July 01, 2015 at 03:27HelloI implemented a cdc_vcp port in stm32f4discovery and tried to communicate with matlab, but matlab can't open the port(com14 in my laptop).What is the problem?Thanks.

Switching between SPI mode 0 and 1?

Posted on July 03, 2015 at 12:48 I have a number of devices connected, some sample the data on the rising clock edge, others on the falling edge. Inside the handler structure I want to alternate between these two operation modes. A method...

STM32L4 SPIs Maximum clock.

Posted on July 02, 2015 at 18:38Hi,For STM32L4.I would like to know if SPI2 and SPI3 maximum clocks are also 40MHZ or only SPI1 clock is?Ari.

Asantos by Senior
  • 1290 Views
  • 2 replies
  • 0 kudos

Bad operation in stm32l0xx_hal_tim.c

Posted on June 23, 2015 at 11:07Hello, I do not understand why the TIMER instance is stopped when a specific bloc is stopped. For example, I have 2 output compare channels activated on TIM2 with interruptions. If I use HAL_TIM_OC_Stop_IT in order t...