STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f465vit PA14 swclk pin always reset state.

Dear sir, madami use my new stm32f465vit with my custom Board swclk pin always reset state.PA14 swclk pin always reset state 0v, after i connect 10k resistor swclk and PA13 swdio pin to 3.3v. make it pullup also same PA14 is 0v (VCC)so, I can’t conne...

STM32H755 interrupt issue after secure boot (SBSFU)

I have a firmware running on an STM32H755. All working fine until I added a secure bootloader to the firmware and now the firmware crashes when initialising TIM3.My setup: STM32H755 on custom boardSBSFU (1_Image)Cubeprogrammer and CubeIDE.I've pinpoi...

tstokes by Associate III
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! UCPD Source(X_NUCLEO_SRC1M1) and Sink (X_NUCLEO_SNK)

Hello, We have purchased the following boards recommended by STM in order to work on UCPD Source and Sink applications: 1. Two NUCLEO-G071RB boards 2. One X-NUCLEO-SRC1M1 3. One X-NUCLEO-SNK1M1 We downloaded the repository of board and imported the f...

Sudarshan by Associate II
  • 1943 Views
  • 3 replies
  • 1 kudos