STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX for SW4STM32 : where is c++ compiler ?

Posted on June 07, 2015 at 18:37Hi, I've generated a project with cubeMx for System workbench. Now, I add some c++ classes which does not compile because they are compiled by eclipse with gcc and not g++. Can anyone tell me how to fix this ? I can n...

JulienD by Senior
  • 2465 Views
  • 4 replies
  • 0 kudos

STM32F4xx ''Idle Line'', ''Idle Character'' detection

Posted on July 20, 2015 at 03:10There seems to be an inconsistent usage of the terms ''Idle Line'', and ''Idle Character'' in the STM32F4 reference manual.In my view, I could consider a transmit or receive line that is idle (without a start bit) for...

gahelton1 by Associate III
  • 1289 Views
  • 0 replies
  • 0 kudos

[STM32F0 Nucleo] Developing on Mac OS X

Posted on July 19, 2015 at 23:02Hi,I have a Nucleo Board, STM32F072R8, and I followed thishttps://stm32geek.wordpress.com/2014/10/21/stm32f3discovery-on-mac-os-x-using-eclipse-gcc-arm-and-openocd/ to develop on Mac OS X using Eclipse IDE. Build Proj...

fredvaz7 by Associate
  • 865 Views
  • 0 replies
  • 0 kudos

STM32F7 using the faults

Posted on July 18, 2015 at 23:13Hi,I'm trying to enable the cortex's fault exeptions for my stm32f7 board.Everytime I call   HAL_NVIC_EnableIRQ(UsageFault_IRQn); or try to enable some other Fault I get an Hard Fault.I already tried to access the reg...

Have I blocked my STM32F103 Eval board

Posted on July 19, 2015 at 15:46I have been using the following setup for trying out a few demo programs. I use the jLINK OB. However it appears that I have blocked my STM32 by uploading bad code.Is there some means of resetting the board in the cur...

0690X000006032xQAA.jpg 0690X00000605HzQAI.png

I2C3 configuration

Posted on April 08, 2014 at 20:48Hi I'm working on STM32F401,I configure I2C1 port as an I2C Master at ''init_I2C1(void)'', and I succeed to communicate with the slave side.  Now I'm trying to configure I2C3 port as an I2C Master at ''init_I2C3(void...

gil23 by Associate III
  • 4281 Views
  • 8 replies
  • 0 kudos

STM32F417VGT6 - SWD - Cant connect to target

Posted on July 17, 2015 at 17:44Hello,After my first steps with the discovery board, I designed my very first PCB with a STM32 MCU (STM32F417VGT6), which I intend to program via SWD (SWDIO, SWCLK, GND, 3.3V). Unfortunately I don't get a connection t...

firmen by Associate
  • 2487 Views
  • 5 replies
  • 0 kudos

How a code is executed in stm32/ARM Cortex M controllers

Posted on July 19, 2015 at 08:10I know that when a c program is compiled and flashed it goes into the flash memory and the flash memory contains the text section, initialized variable section and Read only section. So I just want to know when a prog...

STM32F429I-Discovery Missing serial COM?

Posted on July 14, 2015 at 22:12Hi Everyone.I'm having some doubts about the discovery boards.I have a nucleo board and a STM32F429I discovery board (the one with a LCD).In the nucleo board I had next to no problems sending data to the serial monito...

Resolved! STM32 clock configuration

Posted on July 14, 2015 at 07:15I am a beginner in STM32. Recently I surf the Internet and find some codes written by others. They all says that the RCC should be configured at first as follow: 1. Reset the RCC register; 2. Open HSE; 3. Wait for HS...

Yihao Guo by Associate II
  • 3383 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.