STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746 lacks bit-banding?

Posted on July 20, 2015 at 21:53Does the new STM32F7 series omit bit-banding support?There is no mention of bit-banding in the STM32F7 reference manual.  Attempting to use bit-banding results in a fault condition.I'm surprised by this omission.  Or ...

dale by Associate III
  • 1792 Views
  • 4 replies
  • 0 kudos

STM32L053 discovery standby

Posted on July 20, 2015 at 21:42I write some code that seems to successfully put the chip into standby mode:    PWR->CR |= PWR_CR_PDDS;    SCB->SCR |= SCB_SCR_SLEEPDEEP;    while (1) { __asm(''WFI'')__; }That seems to stop everything as expected. Wh...

lee23 by Associate II
  • 946 Views
  • 2 replies
  • 0 kudos

STM32F072 - Hard Fault when reading from System Memory

Posted on July 20, 2015 at 19:47Hi.I'm looking for some help with the STM32F072.Q: What are you trying to do?A: I'm trying to read the factory measured voltage of the bandgap voltage reference in order to calculate the VDD as exactly as possible. As...

bjerman by Associate II
  • 2803 Views
  • 6 replies
  • 0 kudos

VDDA starts after VDD

Posted on July 20, 2015 at 11:02In the http://www.st.com/web/en/resource/technical/document/application_note/DM00115714.pdf is written: ...During the startup phase VDDA must arrive first and be greater than or equal to VDD. ... Why that what if it i...

stst9184 by Associate II
  • 6263 Views
  • 11 replies
  • 1 kudos

STM32f4 5V output pin

Posted on July 20, 2015 at 12:42Hi, I'm connecting stm32f4-disco through USB to the computer and I'm measuring the 5v output pin from the board with a scope and I get 3,9 V. Did I burn it or something? Thank you

fiulala by Associate II
  • 2603 Views
  • 5 replies
  • 0 kudos

STM32F411RE - RTC and VBAT

Posted on July 20, 2015 at 15:47 Hello I have been trying to get the RTC to work with VBAT. I have connected 3V coin cell battery to the VBAT pin (RTC initialized beforehand). I test if RTC is working in the following way: if((RTC...

tbnkr by Associate II
  • 1651 Views
  • 3 replies
  • 0 kudos

STM32f4 Discovery EXTI Clear pending bit

Posted on July 20, 2015 at 00:05Hello all,I tried searching for a bit but couldn't find anything pertaining to my question.I'm trying to set up an external interrupt but I don't understand why exactly we clear the pending bit in EXTI->PR and not in ...

Setup a USB module (FT232) with a STM32F103 MCU

Posted on July 16, 2015 at 18:21Hi all, I have a STM32F103VEH MCU which is connected to a FT232 USB module. All pins at the MCU with alternate functions are connected to the corresponding pins at FT232 USB module, which are: PA11 -> USBDM (USB data ...

danesh by Associate II
  • 4237 Views
  • 9 replies
  • 0 kudos

Missing Byte VCP example

Posted on July 07, 2015 at 16:40Hello everyone,I'm facing a problem in which I'm clueless how to solve. Maybe someone can help me out or give me some hints.To the setup:I'm running two STM32, one STM32F0 to communicate via USB with a PC and a STM32F...

p23 by Associate II
  • 1130 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.