cancel
Showing results for 
Search instead for 
Did you mean: 

low speed GPIO for FMC?

Tamas Novak
Associate III
Posted on December 27, 2014 at 11:11

HAL_FMC_MspInit()  generated by F4 CubeMX   initializes all FMC related pins as

GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

 

SDRAM is driven at max 84MHz frequency (STM32F429). I know that SPEED_LOW is only a slew rate (~a lower current generator at output driver), and traces to SDRAM are short and low capacitance, so they may be toggled quickly even with low driving power.

Isn't it a problem?  (It's a newly designed board; I haven't tested it yet)

#fmc-gpio-speed-cubemx
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0