STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L0 in UFQFPN32 with HSE

Posted on August 15, 2015 at 11:08Hi, I am looking for an STM32 which has:- A 5x5 mm package which can be used on a 2 layer board (that excludes BGA, I suppose)- 32 or more pins- Ultra low power- DAC- Crystal main clockIn the parametric selection, t...

soren by Associate II
  • 1481 Views
  • 2 replies
  • 0 kudos

STM32F7 discovery kit problem with QSPI

Posted on August 15, 2015 at 10:41Hello, I'm using the STM32F7 discovery kit from ST with Keil uV5, the kit is great however I tried to reload the demonstration firmware, Keil always reports that ''no algorithm found for: <all address in QSPI memory...

Pin termination normally & after power up STM32

Posted on August 14, 2015 at 12:22I am using STM32F205 LQFP64 & want to know if below configuration of pin are ok. I use SWD method.I have grouped pins as:1. vbat:  If not used, connect it to Vdd & decouple by 0.1uf cap.2. PA0-PA15: If any of pin is...

window watchdog example for stm32f103

Posted on August 15, 2015 at 09:59hi every one. i am trying to initial wwdg of stm32f103rbt6 & i am using cmsis libraries for this. based on cmsis examples i wrote my program & it compiled succesfully but dose not work correctly. i attached example,...

mhdizgah by Associate II
  • 1312 Views
  • 1 replies
  • 0 kudos

STM32VLDISCOVERY Keil Assembly Project from Scratch

Posted on June 28, 2013 at 05:44I require to build an assembly project in the STM32VLDISCOVERY board either using Keil's  startup file (startup_stm32f10x_md_vl.s) or no startup file at all. The project must have either absolute (preferably) or reloc...

fj by Associate
  • 3920 Views
  • 7 replies
  • 0 kudos

Software trigged DMA!

Posted on August 15, 2015 at 08:09 STM32F103C8 What is the proper setup of a software trigged DMA? Or how do one setup TIM4 so software trigger DMA works? I get a conflict between TIM4 CCR1 match triggered DMA (which works pe...

STM32CubeMX 4.9.0 and STM32f429-Discovery USB CDC VCP

Posted on August 14, 2015 at 22:24Hi,I have created a USB CDC project using STM32CubeMX. It is running on STM32F429 board. However after receiving first character, the program is not accepting anything. Did anybody face similar problem?Regards,Prova...

provat by Associate II
  • 1467 Views
  • 2 replies
  • 0 kudos

SOLVED: Intermittent ''No ST-Link detected'' message

Posted on August 04, 2015 at 22:44So, I'm having the same problem with the ST-Link driver as those in the past. Sometimes the driver works and I am able to connect via the ST-Link Utility and IAR Workbench. When it does not work, I cannot connect to...

Any SPDIF STM32F7 example project?

Posted on August 06, 2015 at 19:30Hi, Searched the STM32Cube_FW_F7_V1.1.0 library but could not find an example for the SPDIF interface. Is there any example somewhere that I could use for the SPDIF Rx connection? Regards, Christos

sv1eia by Associate II
  • 1553 Views
  • 3 replies
  • 0 kudos