cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F446 Quad SPI pinout

Asantos
Senior
Posted on January 22, 2015 at 12:35

Hi,

  I would like to know what is the difference between the pins QUADSPI_BK2_IO3(PE10) and QUADSPI_BK1_IO3 (PA1)?

  There are only one quadspi interface on the STM32F446, why BK1 and BK2? 

  

  Can I use the pins QUADSPI_BK1_IO1 and QUADSPI_BK2_IO3 for the same quad spi flash memory?

 Ari.

  

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 06, 2015 at 10:45

Hi Ari,

The STM32F446 Quad SPI allows to interface 2 memories. 

So to intterface only one memory, you may use BK1 or BK2.

If 2 memories are required, then you have to configure both pins.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.