STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing a CIS with STM32F

Posted on August 16, 2015 at 23:54Hello everyone,I have a project in which I am using a Contact Image Sensor. I receive an analog signal at 4 MHz which represents the color of a pixel. I have to transform it into a digital signal of 8 bits ( this re...

ed_62 by Associate II
  • 3309 Views
  • 5 replies
  • 0 kudos

System crash with all core registers value as 0xFFFFFFFF

Posted on August 17, 2015 at 08:59I have a system(freeRTOS) running well on stm32f401 platform. To reduce the PowerConsumption, i added a HAL_PWR_EnterSLEEPMode() into the void vApplicationIdleHook( void ). The system will crash in seconds with all ...

bzhang by Associate
  • 635 Views
  • 1 replies
  • 0 kudos

STM32F407 - Multi-ADC mode with DMA

Posted on January 09, 2014 at 15:19How is the DMA supposed to work with Triple-ADC Regulare mode? The documentation shows an ADC stream for each ADC, but it also seems to indicate that it will be working with a single DMA stream for this process. ...

dibs by Associate II
  • 4085 Views
  • 10 replies
  • 0 kudos

STM32Cube F4 USB CDC Rx only once!

Posted on August 14, 2015 at 09:54HW board is stm32f429I-Discovery (MCU: stm32f429ZIT6).I use STM32Cube MX V4.9 and stm32f429 firmware package V1.7 to generate source code of USB CDC function. GUI select device_only mode, and HSE to external 8MHz cr...

tristan by Associate
  • 1030 Views
  • 2 replies
  • 0 kudos

Forum participation by ST

Posted on October 01, 2012 at 16:10Would it be possible for ST, it's technical staff, or FAE's to participate in this forum in a more meaningful way? #evertdekker.com

STM32F4 DISCO and CS43L22 DAC

Posted on August 11, 2015 at 07:59Hey everybody :) The STM32F4 disco has an external audio DAC witch is still a little hard to grasp for me, I was hoping anybody of You know any good tutorials, where it would explain how to get a sampling frequency ...

matas by Associate II
  • 1359 Views
  • 3 replies
  • 0 kudos

GPIO_analog vs ADC, STM32F2

Posted on August 16, 2015 at 09:401. Microxplorer gives option to set any GPIO pin as GPIO_analog or pin as ADC if it has ADC feature.2. What is diff between two. I know abt ADC but what does GPIO_analog do?