STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F407 Ethernet inicialization problem with Uvision4

Posted on August 12, 2015 at 20:09Hi,I am using STM32F407 with uvision4, RL-TCPnet from keil and I have a problem in the Ethernet inicialization.When I turn on the PC and turn on the board at the same time the Ethernet doesn’t work, but if I turn on...

felipe by Associate II
  • 2264 Views
  • 4 replies
  • 0 kudos

STM32F303VC USB-HID

Posted on August 14, 2015 at 10:17Hi,I have got an example about USB for this board. You can control the cursor's direction with this board's mems. But i want to do the reverse of this. Forget mems. I just want to turn on leds with moving the cursor...

CMSIS, STM lib. and OS

Posted on August 12, 2015 at 13:22I have made some program using STM standard peripheral libraries (which uses CMSIS?). I do not use any OS now. I read that CMSIS support RTX and Keil ARM-MDK contains RTOS. I have some elementary questions.1. What m...

hospodar by Associate III
  • 1231 Views
  • 1 replies
  • 0 kudos

Need to use JTAG pin PA15 as Ext Interrupt in STM32F429

Posted on August 14, 2015 at 11:17Hello,Kindly guide me to resolve this.I have a board having STM32F429 on it. while adding new requirements in the board, a situation has arised such that i am left with no option other than to use port pin PA15 for ...

jagdish2 by Associate II
  • 827 Views
  • 0 replies
  • 0 kudos

ST32F4: DRAM throughput

Posted on August 14, 2015 at 01:31Hi allI use the STM32429I-EVAL1 board and I did some memory performance measurements (no DMA). The results were a bit strange, as writing to memory is about 50% faster than reading:@180MHz             write mbs/read...

Generating single pulse on GPIO pin

Posted on July 12, 2012 at 11:25I want to generate single pulse with given length on GPIO pin on STM32F4 Discovery kit. I wanted to use timer in OnePulse mode. So I was planning to use TIM4 and TIM12, becouse I need 6 independent pins for pulses. Bu...

honza by Associate II
  • 7087 Views
  • 11 replies
  • 1 kudos

Srf02 on STM32F4-Discovery per I2C and show on Computer

Posted on August 13, 2015 at 15:46Guten Tag,ich habe nur einen SRF02, der ich mit einem STM32F4-discovery verbinden m�chte.Wie kann ich die gemessene entfernung auf Computer bekommen?K�nnen Sie mir vielleicht hefen bei einem programm code f�r CoIDE?...

wilsan01 by Associate
  • 1061 Views
  • 1 replies
  • 0 kudos

USART on STM32F4 discovey Board

Posted on August 11, 2015 at 12:30Hi all...,,I have an stm32f429zi based discovery board with me and newly woking on ST series. Actually I want to run USART/UART on my board to enable serial communication with other devices..but I am facing a troubl...

maharaj by Associate II
  • 1482 Views
  • 2 replies
  • 0 kudos