User Activity

Hello,I have created a stm32cubeide project and wanted to add my own library folder to that project so I just drag and dropped it into workspace. This library folder will have multiple subfolders and .c/.h files. I linked folder using Includes, .c fi...
Hello, I am trying out a 220 V power measurement set up with 3 STPM34 evaluation boards. I need to use as less wires as possible, so I am using SPI with 3 different CS and 1 SYN pin. I am also trying to reduce component count by using only 1 CLK sour...
Hello,I am using ADC1 channel 1, 3 and 5. All these three inputs are connected to different sensors and I want to create a driver to read those sensors. The problem is that I don't want to read all input channels at once, I want to be able to select ...
Kudos given to