STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Having Issues with classic CAN on STM32H745

Hello Team,We got our board booted up recently and Currently testing out CAN with classic mode. All our external devices support Classic CAN mode and even after configuring it with 500kps, It doesn't seem to transmit data.Please, find the attached MX...

PavanOggu_0-1734438697316.png

SRST error when trying to run openocd on stm32f4

i got a stm32f4 and wrote some code to it, then tried to run openocd  and got this error my openocd.cfgnote - i reflashed the stlink a couple of times and changed it to jlink(and then back to stlink) so that might have something to do with it.would v...

penjo989_0-1729110559801.png penjo989_1-1729110589100.png
penjo989 by Associate
  • 1119 Views
  • 2 replies
  • 0 kudos

Resolved! TRACECLK freq. in STM32H5

I do not see any information on the datasheet or reference manual, how is the TRACECLK in STM H5 (particularly 563 if it matters) derived ? Is the TRACECLKIN SYSCLK or FCLK ?

mete by Senior II
  • 1858 Views
  • 3 replies
  • 0 kudos

External ADC Sampling with DMA (Timing & Configuration)

 Hi everyone,I’m working on a project using an STM32 microcontroller (STM32H745IITx), and I’m trying to set up a DMA transfer for an external 12-bit, 20 MSPS ADC with a 12-bit parallel interface. On my custom board, the data pins of the ADC are route...

ZIMMI99 by Associate
  • 2651 Views
  • 3 replies
  • 0 kudos

STM32F070 ADC single channel issue

Hi,Recently I started working on stm32F07 microcontroller. I am trying to read sensor value using ADC.Issue: ADC value is keep on changing randomly(means its not holding value).Below is my code. Please refer it and help me to figure out the issue.Clo...

0693W00000BbDjWQAV.png
VDutt.1 by Associate
  • 2212 Views
  • 3 replies
  • 0 kudos

SDMMC trace length mismatch

Posted on May 11, 2018 at 01:27 Hi ThereI was looking at AN4661, pg 45 where the signal routing guidelines for SDMMC is given. It has the below bullet points when it comes to skew  The skew being introduced into the clock system by unequal trac...

Resolved! Float value implementation and debugging

Is there a proper way to implement a float value? When i try to declare a float variable and debug via the variables tab and or live expression (global variable) I keep getting incorrect values in some instances. I have included the float library and...

NoviceStm32_0-1734424900179.png NoviceStm32_1-1734424937178.png NoviceStm32_2-1734424981648.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.