STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

adc error handler

hiim using stm32g474vet6timer1 is trigger mode ,timer3 slavemode, both timer1 and 3 operate at 5khztimer1 will trigger timer3 and timer3 will trigger adc at every 5khz ,im using adc in multimode dma ,now the problem is when initally i start these con...

FSMC Connection

Hello teamI'm working on the LCD display parallel connection stm32f4 series.Please check the FSMC interface; I've included my schematic. 

Resolved! CEC TV emulate with STM32, how id setup?

We for testing CEC client device require emulate master. In normal device code we set hcec.Init.OwnAddress = CEC_OWN_ADDRESS_x but for TV master how is right choice?  hcec.Init.OwnAddress = CEC_OWN_ADDRESS_NONE; or hcec.Init.OwnAddress = CEC_OWN_ADDR...

MM..1 by Chief III
  • 1587 Views
  • 3 replies
  • 0 kudos

Resolved! HAL_CAN_AddTxMessage() contains problems

Hi I am using CAN in STM32F303RDT6.I am using HAL_CAN_AddTxMessage for CAN transmission.This function will send the data and return HAL_OK if the sending mailbox is free.However, although HAL_CAN_AddTxMessage returns HAL_OK, no message may actually b...

Ukazu by Associate III
  • 3635 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 UART TEACK forever after clock switch

Hey together,I discovered a super strange a critical behaviour of the STM32H750 chip. Maybe you can help me to prove this issue. We have a firmware which is split into 2 parts (bootloader, application). Both BL and APP are using the UARTs to communic...

bl1.png app1.png
ESawa.1 by Senior
  • 3283 Views
  • 8 replies
  • 1 kudos

Flashing issue using Zephyr & STLink

Hello,We are migrating to zephyr, the board which is supported by zephyr is nucleo_g0b1re, but out actual controller is stm32g0c1ret3. Both are of same family, have same memory and all. I have just made changes in the overlay file for my application,...

Resolved! Setting GPIO interrupts for two identical pins

We are developing a software application that uses GPIO interrupts.We want to set interrupts on the same pins (PE8, PG8), but only one of them can be set to external interrupt mode in the ioc.Is it not possible to set external interrupt mode for two ...