STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743 Dual mode ADC in 8 bit resolution

Hi Experts! Summary: Question: Anyone know if the dual 8bit ADC mode is broken on the STM32H743 or what I could be doing wrong?Details:I am trying to get 8 bit dual mode ADC working on the STM32H743. I see one post on here that seems to indicate some...

image.png image.png
JShro by Associate III
  • 1552 Views
  • 2 replies
  • 0 kudos

adc error handler

hiim using stm32g474vet6timer1 is trigger mode ,timer3 slavemode, both timer1 and 3 operate at 5khztimer1 will trigger timer3 and timer3 will trigger adc at every 5khz ,im using adc in multimode dma ,now the problem is when initally i start these con...

FSMC Connection

Hello teamI'm working on the LCD display parallel connection stm32f4 series.Please check the FSMC interface; I've included my schematic. 

Resolved! CEC TV emulate with STM32, how id setup?

We for testing CEC client device require emulate master. In normal device code we set hcec.Init.OwnAddress = CEC_OWN_ADDRESS_x but for TV master how is right choice?  hcec.Init.OwnAddress = CEC_OWN_ADDRESS_NONE; or hcec.Init.OwnAddress = CEC_OWN_ADDR...

MM..1 by Chief III
  • 1562 Views
  • 3 replies
  • 0 kudos

Resolved! HAL_CAN_AddTxMessage() contains problems

Hi I am using CAN in STM32F303RDT6.I am using HAL_CAN_AddTxMessage for CAN transmission.This function will send the data and return HAL_OK if the sending mailbox is free.However, although HAL_CAN_AddTxMessage returns HAL_OK, no message may actually b...

Ukazu by Associate III
  • 3595 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7 UART TEACK forever after clock switch

Hey together,I discovered a super strange a critical behaviour of the STM32H750 chip. Maybe you can help me to prove this issue. We have a firmware which is split into 2 parts (bootloader, application). Both BL and APP are using the UARTs to communic...

bl1.png app1.png
ESawa.1 by Senior
  • 3224 Views
  • 8 replies
  • 1 kudos

Flashing issue using Zephyr & STLink

Hello,We are migrating to zephyr, the board which is supported by zephyr is nucleo_g0b1re, but out actual controller is stm32g0c1ret3. Both are of same family, have same memory and all. I have just made changes in the overlay file for my application,...