STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Injected ADC timing discrepancy

Hi!I am experiencing some confusing behaviour on an STM32H743 series chip:I am running an injected ADC channel on ADC2, with trigger from the HRTIM. The HRTIM is triggering at 8000 Hz (200 MHz clock, prescaler div-2 and period = 12500). The ADC gener...

MrPylonz by Associate II
  • 2867 Views
  • 7 replies
  • 1 kudos

Contact DRAM operation using STM32H723ZGT6 OSPI1

Hello We are working on a new project with STM32H723ZGT6. I want to control S70KL1283DPBHI020 DRAM with HYPERBUS communication using OSPI1. If you access 0X900000 memory to write and read data during the current operation, the data will not be read a...

IMG123.png IMG345.png
GGIL.1 by Associate II
  • 328 Views
  • 3 replies
  • 0 kudos

MCU stuck - when reach high temp, about 85C

Hello,In our application there is a STM32L073CZT3 component, we use timers and DMA to generate PWM that simulates a sine wave to start a motor.We encounter a problem with the microcontroller at high temperatures (about 80 degrees Celsius and above).T...

OrenS by Associate
  • 292 Views
  • 1 replies
  • 1 kudos

Resolved! RTC is running extremely slowly (3 times too slow)

Hello.   I'm having a problem with an STM32H503. I need to use the RTC, which is running on the internal 32kHz LSI clock. The clock configuration was created with CubeMX.   When I check the RTC, I see that it has only advanced by 21 seconds in 60...

Resolved! STM32H7A3VIH6 Access QSPI

Hello ,I want to Access QSPI drivers in STM32H7A3VIH6. However in Cubemx there is only option of OCTOSPI1 and OCTASPI. My question is there way to use QSPI api directly like HAL_QSPI_Init instead of OSPi init?Or we have use OSPI only?Secondly i am us...

amitpramanik_0-1772694844071.png

Resolved! STM32G473 FDCAN pinout contradiction

Same issue reported in 2020: https://community.st.com/t5/stm32-mcus-products/stm32g473-fdcan-pinout-contradicting/td-p/224770.As of DS12712 Rev 5, Table 13 Alternate Functions has PB10 and PB11 mis-labeled as FDCAN3_RX and FDCAN3_TX respectively.Unde...