cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H733VGT6 can't get interrupts working. Not sure if the problem is in software or in my board.

oyalç.1
Associate III

I am trying to drive a lc resonator from a h bridge. Frequency of the resonator changes when inductor is loaded. 

TIM15 creates the complimentary PWM for the H bridge. I need TIM2 to read the new frequency of the resonator so i can adjust the PWM frequency of TIM15. TIM2 will be reading a square wave.

I tried this guide(and every other one I could find). I tried DMA. I tried interrupts. I even put a breakpoint inside the HAL_TIM_IC_CaptureCallback. It didn't even get triggered.

https://community.st.com/t5/stm32-mcus/how-to-use-the-input-capture-feature/ta-p/704161

At this point i am not sure if my code is wrong or if there is an actual problem with the board. 

Would it be possible for someone to send me a code for TIM2 interrupt that is confirmed working or test my code on a stm32 that is confirmed good?

I am questioning my sanity. The board programs and debugs just fine. cubeide or cubeprogrammer gives no error codes.

here is all the edits I have done to my main.c file

/* USER CODE BEGIN 0 */
uint32_t H_freq;
uint32_t ARR_tim15;
uint32_t frequency;


uint32_t captureValue = 0;

uint32_t previousCaptureValue = 0;

uint32_t frequency = 0;
float freq;
float duty;
float TIMER_CLOCK_FREQ;
/* USER CODE END 0 */



  /* USER CODE BEGIN 1 */
void pwm_frequency_set()  //H bridge pwm frequency
{

				 ARR_tim15=80000000/H_freq;
				  TIM15->ARR = ARR_tim15;        // counter period for timer 15
				  TIM15->CCR1 = ARR_tim15/2;     // duty cycle for timer 15

				  return;
}

void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim) {

	H_freq = 20000;
	  	pwm_frequency_set();


if (htim->Channel == HAL_TIM_ACTIVE_CHANNEL_1) {

captureValue = HAL_TIM_ReadCapturedValue(htim, TIM_CHANNEL_1);

frequency = HAL_RCC_GetPCLK1Freq() / (captureValue - previousCaptureValue);

previousCaptureValue = captureValue;

}

}

  /* USER CODE END 1 */


  /* USER CODE BEGIN 2 */
HAL_TIM_PWM_Start(&htim15, TIM_CHANNEL_1);
HAL_TIMEx_PWMN_Start(&htim15, TIM_CHANNEL_1);
HAL_TIM_IC_Start_IT(&htim2, TIM_CHANNEL_1); // Primary channel - rising edge
HAL_TIM_IC_Start(&htim2, TIM_CHANNEL_2);    // Secondary channel - falling edge

  /* USER CODE END 2 */


  /* USER CODE BEGIN WHILE */
H_freq = 10000;
  	pwm_frequency_set();
 	  while (1)
{
    /* USER CODE END WHILE */
1 ACCEPTED SOLUTION

Accepted Solutions
oyalç.1
Associate III

problem was that the BOOT0 pin was not soldered properly. after soldering it to GND issue went away.

View solution in original post

5 REPLIES 5
mbarg.1
Lead

We use in many H7xx designs interrupts and work great .

I will be favorable to say it is a sw problem.

But to guess where, try to make a subset of your deisgn, post the code, let us try on our hw and give some better feedback.

I attached the full project as a zip file.  The reason why I am suspicious from hardware is because the microcontroller is soldered to a generic LQFP 100 breakout board. I have added bunch of caps to power pins but some capacitors are as far away as 10mm. . It programs just fine but i still don't trust it.

 

Full project for now is just reading the return frequency and adjusting the output frequency according to it.

 

Let us not waste time - try with a sound board like a Nucleo or other eval board - if it work, then we discuss sw 

only if i had one. i bought this microcontroller like 2 years ago. before my country put up huge import taxes and currency lost a lot of value. a nucleo board would eat up my entire budget for a few months. sadly I am stuck with it.

oyalç.1
Associate III

problem was that the BOOT0 pin was not soldered properly. after soldering it to GND issue went away.