STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L476 ADC trigger on SAI MCLK

Posted on April 12, 2016 at 21:40Is it possible to connect the SAI MCLK signal such that it can be used as a clock into a timer which is counted down to provide an ADC trigger - or are there aliasing issues with the timer? I want an internal ADC to ...

brians by Associate II
  • 786 Views
  • 0 replies
  • 0 kudos

Stm32F7: When is it usefull to enable DCACHE?

Posted on April 12, 2016 at 17:44In my understanding, DTCM, SRAM1 and SRAM2 all offer single cycle access. This leads my to the conclusion, that enabling DCACHE in a situation where there is no slow external memory does not bring any advantage, but ...

Question related to DSI resolution

Posted on April 12, 2016 at 16:49Hello! I am learning how to work with DSI interface on stm32f769 controller. There is one question. Dsi host gets the frame from LTDC interface, the maximum resolution of LTDC is 1024*768, but the maximum resolution ...

TIM5 on STM32F107VC?

Posted on April 12, 2016 at 14:17Folks, I am writing some software on the STM32F107VC, but in the header files there is no trace of TIM5, its interrupt vector etc. From what I can see from the datasheet this time should be on the processor. Am I mis...

DiBosco by Senior II
  • 1383 Views
  • 4 replies
  • 0 kudos

STM32 CubeMX bug tracker/feature request

Posted on March 29, 2016 at 21:05Is there some bug tracker or feature request branch on forum? How can I leave feedback for this software? Anyway, here I'll post my proposition. CubeMX generates initialization of periphery like this:   /* Initialize...

sincoon by Associate III
  • 1129 Views
  • 2 replies
  • 0 kudos

CubeMx RTC Timeout does not trigger ISR

Posted on November 28, 2015 at 18:00Hello all, I made a new project with latests CubeMx 1.9 for stm32f4 My problem is that the autogenerated code does not trigger the ISR. I found out that when I __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF...

taraben by Senior
  • 693 Views
  • 2 replies
  • 0 kudos