cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F07x, STM32F08x and STM32F09x are dummy products???

Osto
Senior
Posted on November 06, 2015 at 13:19

Hi,

I have a new project which would run on STM32F051K8T but need more than 64K flash.

I saw the STM32F0[789]x has more flash but nobody sell them!?

Mouser, Digikey,.... have not one of this series.

Do somebody sell them at all? Or are they only on paper?

Regards,

Osto
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief
Posted on November 06, 2015 at 13:44

Try http://www.findchips.com

F072 seems to be available at several places, e.g. Farnell.

Nesrine M_O
Lead II
Posted on November 06, 2015 at 14:32

Hi Osto,

Look to the ST website to have an idea about product distributor availability, for example

http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1574/LN1826/PF261320#

 

-Syrine-