STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DSH I2C understanding

Posted on April 10, 2016 at 19:56Hello Community,I am currently trying to get my head around the LIS3DSH accelerometer using the I2C HAL library, however I am having a great deal off difficulty in achieving anything.My aim is to simply read the axes...

b4038201 by Associate
  • 1160 Views
  • 1 replies
  • 0 kudos

Unable to shut down the USB core

Posted on April 11, 2016 at 17:08I'm currently having some issues with the USB core on the STM32f4. Before enabling the USB core the VBUS line (GPIO A9) is low as would be expected. when a usb cable is plugged it I detect this and enable my USB core...

Timer with external clock in gated mode

Posted on April 11, 2016 at 09:39Hi, I would like to configure a timer as a slave in gated mode which has an external clock from another timer. So in my setup I do would have three timers. A ''clock timer'' which outputs a given clock frequency, a m...

smrtkai by Senior
  • 4120 Views
  • 2 replies
  • 0 kudos

Allocate HEAP into external SDRAM with Keil-RTX

Posted on November 24, 2015 at 09:02 Hello! I'm developing an application which requires the heap to be located in a 32MB off-chip SDRAM. I'm using Keil RTX in the project.The problem is the application falls when a function malloc() is ca...

y_ by Associate
  • 1946 Views
  • 2 replies
  • 0 kudos

Disabling Reset pin on stm32f05X

Posted on April 08, 2016 at 10:34Hi Group,Is it possible to disable the Reset pin on this micro for a time interval so that any external reset pulse don't have any effect during this time?Kind RegardsBob

stenasc by Senior
  • 1576 Views
  • 2 replies
  • 0 kudos

Watch dog reset flag on STM32F051

Posted on April 08, 2016 at 18:43Hello,i'm using a STM32F051 and i want to know if the reset is a watch dog reset or not.I read the flag IWDGRSTF in the CSR register (RCC peripheral) but this bit is always set when a reset occurs.I tried with no wat...

Where is the right way to undersand NAND HAL configuring

Posted on April 11, 2016 at 11:00Hello, dears!I'm stucking around interfacing the NAND to STM32F746The nand is (NAND512W3A2CN6)Thus we have 512 bytes (0.5 kBytes) per Pagebut in the HAL drivers description we can see:PageSize  - NAND memory page (wi...

cqdx by Associate
  • 711 Views
  • 0 replies
  • 0 kudos

need link to download CubeMx 4.14.0

Posted on April 11, 2016 at 08:51Hello, I try to download CubeMx 4.14.0 from ST Webpage, but only always get ''Sorry page not found'' I need the setup program for a restorable development enviroment.

USB HOST (type A) advice

Posted on April 06, 2016 at 12:43Hello everybody!I want a little advice on the best way to code (on a STM32F4) an USB HOST ''ONLY'' with a standard type A connector.The picture of the STM32 > USB CONNECTOR cabling is attached: https://my.st.com//pub...

STM32F103 CAN ERRI bit always set

Posted on February 28, 2016 at 17:43Hello,I have a problem with CAN bus on STM32F103TB.I have CAN_ESR register = 0 but still I get bit ERRI in CAN_MSR = 1.If i try clearing it either via code or via debugger it will be set again by hardware.I've sea...

SPLabs by Associate II
  • 2703 Views
  • 5 replies
  • 0 kudos