Posted on December 24, 2015 at 06:25Hi All,I’m having a problem that I hope folks might be able to assist with. I have built 100s of STM32F1 target based multirotor flight controllers. Never once have I had a problem programming the F1. Decided t...
Posted on December 25, 2015 at 06:14Small Update: Put a USB on the board. Jumped Boot pins. Was able to connect to STM Bootloader via USB and flash F3. Still cannot connect via SWD/UART no matter what I do. Any help/input would be greatly appr...
Posted on December 24, 2015 at 08:53 Thanks Clive for the response. I didn't do a schematic for the breakout board. Just threw it together. Sorry. I've attached the schematic for the F1 board that I put an F3 on. Only populated t...