cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 Disable PWM for protection purpose

minhpc91
Associate II
Posted on December 27, 2014 at 13:38

I'm using Channel 1&3 in TIM1 to generate 4 Complementary PWMs (PA8, PA10, PB13, PB15, STM32F401VC DISCOVERY) to control my FullBridge DC-DC Converter. 

In overcurrent or overvoltage cases, the PWM should be shutdowned to protect the MOSFETs. I'm using the following codes in Read_ADC() Procedure to do that.

I wonder wheather these PWM Pin would be transfer to OpenDrain or connect to GND after shutdowned? And how could I connect GND for these Pins this case? This problem has influenced to the driver circuit and the MOSFETs very much.

Can anyone help me?

Thank you very much!!

// Check Max_Cur and Max_Vb to disable PWM

    if ( Ir_Buf[Cur_Pos] > Max_Cur )

   

        {

   

                    TIM1->CR1  &= (uint16_t)(~TIM_CR1_CEN);

                                    TIM1->BDTR &= (uint16_t)~TIM_BDTR_MOE;

   

                    TIM1->CCER &= (uint16_t)~(TIM_CCER_CC1E | TIM_CCER_CC1NE | TIM_CCER_CC3E | TIM_CCER_CC3NE);

   

        }

            if (Vb_Buf[Cur_Pos] > Max_Vb)

 

                      {

                                    TIM1->CR1  &= (uint16_t)(~TIM_CR1_CEN);

                                    TIM1->BDTR &= (uint16_t)~TIM_BDTR_MOE;

                                    TIM1->CCER &= (uint16_t)~(TIM_CCER_CC1E | TIM_CCER_CC1NE | TIM_CCER_CC3E | TIM_CCER_CC3NE);

 

                      }
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
minhpc91
Associate II
Posted on December 29, 2014 at 07:16

Can anyone help me? This problem can cause some incidents if I dont understand it in the root.

Thank you very much!!