Question
Timer in PWM Capture Mode
Posted on November 23, 2015 at 15:16
Hello every One
I am trying to read PWM signal parameters (Frequency & Duty Cycle) with timer 2 of STM32f4 IC. According to data sheet There is two modes of reading PWM signal.
1- capture mode which reads Pulse widths
2- Pairing Mode with use of two ICs configuration.
Since I am not expert in working with stm32f4, I provided the code mentioned below to read Frequency & Duty Cycle, with the help of other codes written in this forum.
First of all I want to know : Is that possible to read Duty Cycle with the first mode or not, and if yes how it should be done.?!
Secondly when i run the below code I can not read frequency and Duty Cycle as correct as should be. The entrance signal has the frequency of 45 Hz and a duty of 40 percent. \
I think the problem is with the time base configurations in which the prescaler and period should be defined.
I will be Please if someone can help me to overcome above issues.
Thanks.
Soren
void TIM2_IRQHandler(void)
{
RCC_ClocksTypeDef RCC_Clocks;
RCC_GetClocksFreq(&RCC_Clocks);
if (TIM_GetITStatus(TIM2, TIM_IT_CC1)!= RESET)
{
TIM_ClearITPendingBit(TIM2, TIM_IT_CC1);
IC2Value_ = TIM_GetCapture1(TIM2);
if (IC2Value_ != 0) {
DutyCycle_ = (TIM_GetCapture2(TIM2) * 100) / IC2Value_;
Frequency_ = (RCC_Clocks.HCLK_Frequency)/2 / IC2Value_;
} else {
/* Reset data */
DutyCycle_ = 0;
Frequency_ = 0;
}
}
}
/* --------------------------------------PWM Input --------------------------------------*/
TIM_ICInitTypeDef TIM_ICInitStruct;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
// /* --------------------------------------Timer2--------------------------------------*/
/* TIM2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
/* GPIOC clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB, ENABLE);
/* TIM2 GPIO pin configuration : CH1=PA0, C2=PA1, CH3=PB10, CH4=PB11 */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10| GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect pins to TIM3 AF2 */
GPIO_PinAFConfig(GPIOA, GPIO_PinSource0, GPIO_AF_TIM2 );
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM2 );
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_TIM2 );
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_TIM2 );
/* Intrupt Config */
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
/* Time base configuration - SystemCoreClock = 168000000 for 168 MHz board ABP1 @ 42 MHz (DIV4) */
TIM_TimeBaseStructure.TIM_Prescaler = (uint16_t) (((SystemCoreClock / 1000000) / 2) - 1); // Shooting for 1 MHz, (1us)
TIM_TimeBaseStructure.TIM_Period = 0xFFFFFFFF; // Maximal
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
/* Enable capture*/
TIM_ICInitStruct.TIM_Channel = TIM_Channel_1;
TIM_ICInitStruct.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStruct.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStruct.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStruct.TIM_ICFilter = 0;
TIM_ICInit(TIM2, &TIM_ICInitStructure);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0;
TIM_ICInit(TIM2, &TIM_ICInitStructure);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_3;
TIM_ICInitStruct.TIM_ICPolarity = TIM_ICPolarity_Rising;
TIM_ICInitStruct.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStruct.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStruct.TIM_ICFilter = 0;
TIM_ICInit(TIM2, &TIM_ICInitStructure);
TIM_ICInitStructure.TIM_Channel = TIM_Channel_4;
TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Falling;
TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
TIM_ICInitStructure.TIM_ICFilter = 0;
TIM_ICInit(TIM2, &TIM_ICInitStructure);
TIM_PWMIConfig(TIM2, &TIM_ICInitStructure);
// /* Select the TIM2 Input Trigger: TI2FP2 */
// TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);
TIM_SelectInputTrigger(TIM2, TIM_TS_TI1FP1);
// /* Select the slave Mode: Reset Mode */
TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset);
TIM_SelectMasterSlaveMode(TIM2,TIM_MasterSlaveMode_Enable);
/* Enable TIM2 */
TIM_Cmd(TIM2, ENABLE);
/* Enable CC1-4 interrupt */
TIM_ITConfig(TIM2,TIM_IT_CC1|TIM_IT_CC2|TIM_IT_CC3| TIM_IT_CC4, ENABLE);
#stm32f4-timer #mucapture #pwm