User Activity

Hello,I have a solution which I am trying to port to STM32 MCUs which are able to run a machine learning/deep learning model. i wanted to know is it possible to generate a combined network.c from two models? Or do I have to generate multiple network....
Hello, in the X-CUBE-BLE package this document STMicroelectronics.X-CUBE-BLE2_GettingStarted.pdf says the maximum SPI frequency could be 1Mbits/s . In high perf MCU running at SysClock >500 Mhz , is it possibe to interface BlueNRG2 with it?using Cl...
Hello, I am using F401RE Nucleo + X-NUCLEO-BNRG2A1 + IKS01A2 and FunctionPack 4.2.1 .After dragging the _BL_v4.2.0 bin to the nucleo on resetting the board i am getting this : Error: hci_le_set_scan_response_data [ff]while on another board it is givi...
Hello, I am using STM32CubeMX to generate the code and test some peripherals which runs at different clock speeds(optimally).Since there is lot of code I have (specific to application) post STM32CubeMX code generation being written I don't want to re...
Hello , I amusing the Function pack for sensors(IKS01A3) and BLE (BlueNRG2A1) on STM32L476RG but I am constantly getting the below error : Error: hci_le_set_scan_response_data [ff]Full log : UART InitializedSTMicroelectronics FP-SNS-MOTENV1:    Versi...
Kudos from