STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Customize Board with STM32F072RB

Posted on June 12, 2016 at 22:17HiI am going to develop a customize board based on STM32F072RB IC. I am searching for some application circuit, but couldn't find any. However I got some help from STM32F0 Discovery board schematic but it's confusing....

anuj by Associate II
  • 1174 Views
  • 5 replies
  • 0 kudos

RNG clock messing up LTDC

Posted on April 24, 2016 at 14:02Hi,I have configured my stm32f756xx mcu to run LTDC. Everything works fine. However when I activate the RNG clock like so:__HAL_RCC_RNG_CLK_ENABLE();I seem to get a myriad of red pixels (static snow) on the screen (w...

UART baud rate

Posted on June 13, 2016 at 18:50Hi.I communicate between two F303 parts over UART. Both modules are clocked with 72 MHz. USART1 on one part is on APB2, which runs at 72 MHz. On the other part, USART2 is used, which is on APB1 (36 MHz). But USART2 is...

matic by Associate III
  • 1712 Views
  • 3 replies
  • 0 kudos

STM32F205VE CAN Bus-Off recovery problem

Posted on June 08, 2016 at 11:32 Hi, I have a problem with CAN after a bus-off condition. When CAN state changes to bus-off, I set the CAN operation mode to SLEEP mode. After a few 100 ms I try to bring the CAN bus into NORMAL mo...

CubeMX / Http server example dynamic web page - size limits?

Posted on June 13, 2016 at 16:56This is in the http server example in the CubeMX firmware, V1.4.0 for F7.I'm modifying a web page from the original in the DynWebPage function which has a PAGE_START and a PAGE_BODY both specified at 512Bytes.I want t...

tau by Associate II
  • 829 Views
  • 0 replies
  • 0 kudos

HTTP server from cube firmware?

Posted on June 07, 2016 at 09:36Hi,   are there any tutorials for getting an HTTP server working from cube firmware?I found the demo project in the F7 cube firmware V1.4.0 which displays which tasks are running on FreeRTOS. Works fine, great. Now I ...

tau by Associate II
  • 1420 Views
  • 2 replies
  • 0 kudos

Stm32L053R8 Power consumption is 5mAmps

Posted on June 13, 2016 at 14:36Hello,As i am designing a project for low power application. The best microcontroller that i had selected is STM32L053R8 which is cortex m0+. Now after drawing shematics according to my application requirement i found...

0690X000006039PQAQ.jpg
srm by Associate II
  • 1017 Views
  • 1 replies
  • 0 kudos

STM32L476 power consumption not match

Posted on June 13, 2016 at 13:53No peripheral enabled.Only mcu is mounted and power is feed from power supply directly.Current is nearly 170 uA at MSI 1Mhz low power sleep mode.but cubeMx says 65 uA.In other modes, current is almost 100 uA more than...

isjeon by Associate II
  • 1195 Views
  • 1 replies
  • 0 kudos