Question
STM32F429 - CAN stop IT stops firing randomly
Posted on February 08, 2016 at 21:56
Hi,
I'm using a STM32F429 disco board. I used the CubeMX to gen my HAL. Everything works pretty great, except for after a while my CAN IT stops firing. Here is my code below. In the HAL_CAN_RxCpltCallback, the HandleCanEvent does some slight data manipulation then transmits this info back on the bus. It appears that when the CAN bus is very active is when the IT stops firing and I have to reset the Micro. Why would my Interrupt stop firing? Any thoughts?void
HAL_CAN_RxCpltCallback(CAN_HandleTypeDef* CanHandle)
{
HAL_GPIO_TogglePin(GPIOG, LD4_Pin);
// Da activity LED
//Now process crap
canConversionFactory->HandleCanEvent(CanHandle);
/* Receive */
if
(HAL_CAN_Receive_IT(CanHandle, CAN_FIFO0) != HAL_OK)
{
/* Reception Error */
//TODO implement handeling
}
}
void
CAN1_RX0_IRQHandler(
void
)
{
/* USER CODE BEGIN CAN1_RX0_IRQn 0 */
/* USER CODE END CAN1_RX0_IRQn 0 */
HAL_CAN_IRQHandler(&hcan1);
/* USER CODE BEGIN CAN1_RX0_IRQn 1 */
/* USER CODE END CAN1_RX0_IRQn 1 */
}
void
HAL_CAN_MspInit(CAN_HandleTypeDef* hcan)
{
GPIO_InitTypeDef GPIO_InitStruct;
if
(hcan->Instance==CAN1)
{
/* USER CODE BEGIN CAN1_MspInit 0 */
/* USER CODE END CAN1_MspInit 0 */
/* Peripheral clock enable */
CAN1_CLK_ENABLED++;
if
(CAN1_CLK_ENABLED==1){
__CAN1_CLK_ENABLE();
}
/**CAN1 GPIO Configuration
PB8 ------> CAN1_RX
PB9 ------> CAN1_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF9_CAN1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(CAN1_RX0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(CAN1_RX0_IRQn);
/* USER CODE BEGIN CAN1_MspInit 1 */
/* USER CODE END CAN1_MspInit 1 */
}
else
if
(hcan->Instance==CAN2)
{
/* USER CODE BEGIN CAN2_MspInit 0 */
/* USER CODE END CAN2_MspInit 0 */
/* Peripheral clock enable */
__CAN2_CLK_ENABLE();
CAN1_CLK_ENABLED++;
if
(CAN1_CLK_ENABLED==1){
__CAN1_CLK_ENABLE();
}
/**CAN2 GPIO Configuration
PB5 ------> CAN2_RX
PB6 ------> CAN2_TX
*/
GPIO_InitStruct.Pin = GPIO_PIN_5|GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF9_CAN2;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral interrupt init*/
HAL_NVIC_SetPriority(CAN2_RX0_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(CAN2_RX0_IRQn);
/* USER CODE BEGIN CAN2_MspInit 1 */
/* USER CODE END CAN2_MspInit 1 */
}
}
HAL_StatusTypeDef CanDriver::InitializeCan1(BaudRate baudRate)
{
if
(!hcan1)
return
HAL_ERROR;
if
(!baudRate)
return
HAL_ERROR;
hcan1->Instance = CAN1;
static
CanTxMsgTypeDef TxMessage;
static
CanRxMsgTypeDef RxMessage;
if
(baudRate ==
this
->BITRATE_500k)
{
hcan1->Init.Prescaler = 4;
hcan1->Init.SJW = CAN_SJW_1TQ ;
hcan1->Init.BS1 = CAN_BS1_14TQ ;
hcan1->Init.BS2 = CAN_BS2_6TQ ;
}
else
if
(baudRate ==
this
->BITRATE_250k)
{
//TODO
}
else
//Assume 500k
{
hcan1->Init.Prescaler = 4;
hcan1->Init.SJW = CAN_SJW_1TQ ;
// This is for 500k can
hcan1->Init.BS1 = CAN_BS1_14TQ ;
hcan1->Init.BS2 = CAN_BS2_6TQ ;
}
hcan1->Init.TTCM = DISABLE;
hcan1->Init.ABOM = DISABLE;
hcan1->Init.AWUM = DISABLE;
hcan1->Init.NART = DISABLE;
hcan1->Init.RFLM = DISABLE;
hcan1->Init.TXFP = DISABLE;
//Setup the empty Rx/Tx
hcan1->pRxMsg = &RxMessage;
hcan1->pTxMsg = &TxMessage;
HAL_StatusTypeDef can1SetupStatus = HAL_CAN_Init(hcan1);
HAL_StatusTypeDef can1FilterStatus =
this
->InitializeOpenFilters(CANBUS1);
if
(HAL_CAN_Receive_IT(hcan1, CAN_FIFO0) != HAL_OK)
// Start listning
{
return
HAL_ERROR;
}
return
can1SetupStatus;
}
HAL_StatusTypeDef CanDriver::InitializeOpenFilters(
int
bus)
{
if
(bus < 1 || bus > 2)
return
HAL_ERROR;
CAN_FilterConfTypeDef sFilterConfig;
/*##-2- Configure the CAN Filter ###########################################*/
sFilterConfig.FilterNumber = 0;
sFilterConfig.FilterMode = CAN_FILTERMODE_IDMASK ;
sFilterConfig.FilterScale = CAN_FILTERSCALE_32BIT ;
sFilterConfig.FilterIdHigh = 0x0000;
sFilterConfig.FilterIdLow = 0x0000;
sFilterConfig.FilterMaskIdHigh = 0x0000;
sFilterConfig.FilterMaskIdLow = 0x0000;
sFilterConfig.FilterFIFOAssignment = 0;
sFilterConfig.FilterActivation = ENABLE;
sFilterConfig.BankNumber = 14;
if
(bus == CANBUS1)
return
HAL_CAN_ConfigFilter(hcan1, &sFilterConfig);
if
(bus == CANBUS2)
return
HAL_CAN_ConfigFilter(hcan2, &sFilterConfig);
return
HAL_ERROR;
//we should never get here
}