STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About PWR activation when setting clock

 void SystemClock_Config(void) { LL_FLASH_SetLatency(LL_FLASH_LATENCY_4); while(LL_FLASH_GetLatency() != LL_FLASH_LATENCY_4); #if 1 LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_PWR); #endif LL_PWR_SetRegulVoltageScaling(LL_PWR_REGU_VOLTAGE_SC...

treeset by Associate II
  • 2124 Views
  • 2 replies
  • 0 kudos

Resolved! TSC Advice please

Hi, I am working on an IR remote using STM32L412RBT6P. I have the touch sensing system working to provide the buttons for the user. The user touches a button to send an IR (RC5) code and an LED flashes to let you know it happened. Q1:I have one touch...

Lanceh by Associate III
  • 1946 Views
  • 2 replies
  • 0 kudos

stm32h7 uart IDLE

Hi,MCU - STM32h743I have a use case where I need to receive a large chunk of data on UART, and the RX data length is unknown. I have read ST articles about how to do this using the IDLE feature with circular DMA (HAL_UARTEx_ReceiveToIdle_DMA). Howeve...

Daan1 by Associate II
  • 3236 Views
  • 5 replies
  • 0 kudos

Resolved! STM32F7 RS485 DE Enable Not working

Hi I have been trying to configure the RS485 and trying to enable DE line. Though I have configured the DE line correctly, but still when HAL_UART_Transmit() is called, it just stays low and never get enabled for D to tranmit the data to the destinat...

DESTM32 by Associate II
  • 2964 Views
  • 5 replies
  • 0 kudos

Resolved! Has STM32G0b0K system DFU bootloader or not?

STM32G0B0 datasheet DS13565 Rev 3 in Chapter 3.6 Boot modes tells: "• USB on pins PA11/PA12 (except for STM32G0B0KE)" This reads like DFU system bootloader is not available. However AN2606 Rev 64 has no restrictions for DFU bootloader on STM32G0B0. I...

Resolved! STM32F072RBT6 USB Host Device

Hi,I'm using stm32f072rbt6 mcu for my project.And I want to write data to my usb flash drive as a txt file.I have researched some tutorials but to do this usually used mcu's such as stm32f767zit6 and these mcu's have USB_OTG_FS feature which my mcu d...

How to find DMA channel for Timer

We are working on STM32C071KBU6 In STM example TIM_DMA, I see it uses PA10 - TIM1_CH3 with DMA channel 5, but I could not find anything about this. Anyone know how to find this information? I would like to use different pins but don't know what DMA c...

DatTran_0-1736288155168.png
Dat Tran by Senior II
  • 3244 Views
  • 9 replies
  • 2 kudos