User Activity

Hi,I have evaluated various controllers and found that the STM32H725ZGT3 is the best fit for our product due to its memory (both NAND & RAM) size, operating temperature range, secure boot hash features, and ECC capabilities. However, I am unable to l...
Hello ST Community,I am seeking guidance on how to properly configure the VDD50USB and VDD33USB pins on our STM32 device when we are not utilizing the USB functionality. The explanations provided in the datasheet and application notes are somewhat am...
Hi,I have decided to use the STM32H573xx microcontroller. According to the datasheet, there are two versions: one with SMPS and one with LDO. My requirements specify not to use the SMPS, so I chose the STM32H573ZIT3, which does not have the 'Q' suffi...
I have chosen the STM32F765ZIT7 for my project due to its suitable number of pins and bus interfaces. However, this microcontroller does not support Error Correction Code (ECC) for SRAM. Therefore, I kindly request your recommendation for the best re...
Hello,We have a cybersecurity requirement to protect against unauthorized firmware uploads during data load operations or shop load using JTAG. Is there a feature available in the STM32F7xxx family Microcontroller that complies with cybersecurity sta...
Kudos given to