STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX USB_FS_CDC for STM32F407IG

Posted on June 04, 2016 at 05:32Hi everybody,I got a problem to implement USB CDC to STM32F407IG. Although looking into all the post here, still not solve my problem.I am using self-made board with  STM32F407IGT6, The sch is simply connect as MCU US...

Timers with F4 DISCO

Posted on June 23, 2016 at 21:54I want to measure how long a signal is high as accurately as possible (preferably down to the microsecond). I started by triggering an EXTI interrupt one both the rising and falling edge of the signal. The EXTI handle...

I2C start condition not working

Posted on June 23, 2016 at 20:11 I am working on getting familiar with the STM32F411 using ST evaluation board STM32F411E-DISCOVERY. I have written the following code using Eclipse + Ac6 STM32 + gcc (arm-none-eabi5.3 2016q1) I am a...

How to implement HAL_CAN_RxCpltCallback()

Posted on June 23, 2016 at 17:03I am a little confused with this call back function HAL_CAN_RxCpltCallback().  The end users are supposed to implement this function but there is already one in the file: stm32f0xx_hal_can.c.  STM recommends do not mo...

Vu.Andy by Associate III
  • 1245 Views
  • 1 replies
  • 0 kudos

Help me about custom board based-on STM32F746G-DISCO.

Posted on June 22, 2016 at 14:40Hi all,I have a custom board based-on stm32F746G-DISCOVERY. I connect my board to ST-LinkV2 over SWD. I can dectect stm32f7 chip, but I can't flash it to 0x08000000 address. ST-Link Utility report :19:22:39 : ST-LINK ...

Nucleo-144 DMA Memory to Memory Transfer not working

Posted on June 23, 2016 at 16:01 I am trying to configure the DMA2 using the registers and I cannot get the DMA to work. I must be having a bad day because nothing seems to be working correctly. Here is my simple code that does not...

STM32F091 UART1 Wake-UP from stop mode

Posted on June 17, 2016 at 14:03 I've been trying to get this beast to wake up from stop mode when it received data on UART1. This is my approach in code int main() { SystemCoreClockUpdate(); initStopMode(); initUart(); //Init othe...

b239955 by Associate II
  • 2630 Views
  • 5 replies
  • 0 kudos

Can't build an example from ST

Posted on June 17, 2016 at 14:45Hi, I'm facing problem with one of St's example, this one http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-ble1.html#get...

quentin23 by Associate II
  • 1012 Views
  • 1 replies
  • 0 kudos