User Activity

Posted on January 19, 2018 at 10:34Hello i have any question about Comp in STM32F31. What is the propagation delay for low overdrive, for example 5mV? In DS is only for 100mV. For High speed mode.2. What is the output current for Low and high level ...
Posted on September 20, 2017 at 17:34Hello I find ''minor discrepancy'' between datasheet and CumeMX, alee last releas.In DS is NPOR pin on position 20 LQFP48 and in CubeMX in position 43.  and in DS is on 43 P7B and in CubeMX PB2 on 20 .
Posted on January 17, 2017 at 09:38I find http://www.bdtic.com/DownLoad/ST/AN4023.pdf STM32 secure firmware upgrade (SFU) overview , AN is unfortunately from 2012 and ending sentence 'For more details about the complete solution, please contact your...
Posted on December 19, 2015 at 11:44In STMCubeMX I found new subfamily STM32L011 in small package TSSOP14 and UFQFPN20. When will theseprocessorsavailable? You're not going STM32, which would compete with processors PIC12 and PIC10 from Microchip. ...
Posted on December 06, 2015 at 13:35I have a few questionsforthe designand choiceof crystals 1. 32.768kHz. In datasheet is Recommended load capacitance max 15pF In AN2586 is ''To avoid exceeding the maximum value of CL1 and CL2 (15 pF) it is strongl...