STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ITM configuration for SWD print

Posted on July 25, 2016 at 08:42Hello, We are using STM32l476 uC with Jlink segger debugger, and trying to print logs through ITM to Segger J-Link SWO Viewer , the 48 MHz HSE clock is being used as sysclk with RCC_PLL_NONE, We are using   ITM_SendCh...

Difference between STM32F429i-DISCO & STM32F429i-DISC1

Posted on August 04, 2016 at 14:50Hi y'alldoes any one know the difference between STM32F429i-DISCO & STM32F429i-DISC1 that may be causing the issue I have & how to get around it ?basically I've been using a STM32F429i-DISCO to build a demo unit for...

daemynnur by Associate II
  • 3229 Views
  • 6 replies
  • 0 kudos

FMC NAND problem

Posted on August 05, 2016 at 12:06Hi, I have a problem when you use the microcontroller STM32F746(NUCLEO-F746ZG)   FMC together with the NAND memory K9F1G08U0E. The documentation states that it is sufficient to read the data at the address 0x8000000...

Konmax by Associate II
  • 745 Views
  • 1 replies
  • 0 kudos

STM32L476VGT6 pin PC13 odd behaviour

Posted on August 05, 2016 at 00:16We have had an odd problem with using pin PC13 as an output GPIO (for active-low chip-select of a bit-banged SPI).  (PC13 is not defined as a GPIO_EXTI13.)  We found that controlling this GPIO somehow leads to USB (...

timers clock divider on STM32f103

Posted on August 05, 2016 at 10:53hi,I just found that clock devider not work for some Frequency, for example if PLL is used without divider, Timer clock cant be devided. EnjoyAll the best, #stm32 #timer #interrupt

miroslav by Associate III
  • 665 Views
  • 0 replies
  • 0 kudos

STM32F746, ADC

Posted on August 03, 2016 at 08:43Hello, can someone to explain to me what happen when you use 8 channels on ADC, and use DMA. How DMA take ready sample from data register. I think when first channel is ready, dma take it first, after that second, t...

Unstable I2C on STM32F746 Discovery

Posted on July 31, 2016 at 16:04 I've been struggling with this problem for weeks now. Basically I am trying to read out a sensor via I2C. The L3SD I am reading out the sensor in FreeRTOS, but the sensor readout task has the highest priority of a...

about changing RTC wakeup counter in run time

Posted on August 05, 2016 at 05:04Dear all,I am using stm32L151VD.I got an application which needs to change the RTC wakeup counter reload value in run time. My original wake up period is 1/16s. And then I use the code below to change the wake up pe...

jones by Associate
  • 900 Views
  • 0 replies
  • 0 kudos