cancel
Showing results for 
Search instead for 
Did you mean: 

disable interrupt

mauro2
Associate II
Posted on January 18, 2016 at 17:14

i know how to set properly timer interrupt and it works fine. now i'm trying to create a function to disable interrupt. i should be something like this:

void TimDisableInterrupt(TIM_TypeDef* TIMx)

{

switch((int)TIMx)

{

case (int)TIM2:

NVIC_DisableIRQ(TIM2_IRQn);

break;

case (int)TIM3:

NVIC_DisableIRQ(TIM3_IRQn);

break;

case (int)TIM4:

NVIC_DisableIRQ(TIM4_IRQn);

break;

case (int)TIM5:

NVIC_DisableIRQ(TIM5_IRQn);

break;

case (int)TIM6:

NVIC_DisableIRQ(TIM6_IRQn);

break;

case (int)TIM7:

NVIC_DisableIRQ(TIM7_IRQn);

break;

default:

break;

}

NVIC_InitTypeDef nvicStructure;

nvicStructure.NVIC_IRQChannelCmd = DISABLE;

NVIC_Init(&nvicStructure);

TIM_ITConfig(TIMx, TIM_IT_Update, DISABLE);

TIM_Cmd(TIMx, DISABLE);

TIM_ClearITPendingBit(TIMx, TIM_IT_Update);

}

so TimDisableInterrupt(TIM6) should disable TIM6 interrupt, but it doesn't work and it continue to go inside here:

void TIM6_IRQHandler(void)

{

    if (TIM_GetITStatus(TIM6, TIM_IT_Update) != RESET)

    /*do something */

    TIM_ClearITPendingBit(TIM6, TIM_IT_Update);

}

why?

i'm using stm32f10x
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Radosław
Senior III
Posted on January 19, 2016 at 12:43

Your interrupt handling isn't good. Clearing flag at the end i bad idea. You will get multiply handler execution per 1 event.

__disable_interrupts()

_ISB();         -> this can be very important.  this bloks next intruction untill interrupt will be disabled.

some_instruction