STM32F4-Discovery RTC only counting in debug
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-17 1:04 PM
Hello. I am having a bit of a problem using the RTC in the STM32F4-DISCOVERY board. I am using the HAL libraries, and have configured the RTC using the LSI based on a number of examples I found online. Basically I am sending some information wirelessly to another system, which contains the time that information was generated. However the RTC only seems to work in debug mode. When I get out of debug mode, it seems that the RTC is stopped and the remote system receives always the same date. Any ideas on why this is happening? Here is the code I use to configure the clocks and the RTC:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK|RCC_CLOCKTYPE_PCLK1
|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
void RTC_ClockConfig(){
RCC_OscInitTypeDef osc_init;
RCC_PeriphCLKInitTypeDef perif_init;
osc_init.PLL.PLLState = RCC_PLL_NONE;
osc_init.OscillatorType = RCC_OSCILLATORTYPE_LSI;
osc_init.LSIState = RCC_LSI_ON;
perif_init.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
HAL_RCC_OscConfig(&osc_init);
HAL_RCCEx_PeriphCLKConfig(&perif_init);
__HAL_RCC_RTC_ENABLE();
}
void RTC_Init(void){
rtc_handle.Instance = RTC;
rtc_handle.Init.HourFormat = RTC_HOURFORMAT_24;
rtc_handle.Init.AsynchPrediv = RTC_ASYNC_PREDIV;
rtc_handle.Init.SynchPrediv = RTC_SYNC_PREDIV;
rtc_handle.Init.OutPut = RTC_OUTPUT_DISABLE;
rtc_handle.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
rtc_handle.Init.OutPutType = RTC_OUTPUT_TYPE_PUSHPULL;
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnableBkUpAccess();
RTC_ClockConfig();
__HAL_RCC_RTC_CONFIG(RCC_RTCCLKSOURCE_LSI);
__HAL_RCC_RTC_ENABLE();
HAL_RTC_Init(&rtc_handle);
}
#stm32f4-rtc-rcc-lsi
- Labels:
-
RTC
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-18 6:02 AM
A little update. Only when I am watching the registers in the KEIL debug peripherals viewer it works. Otherwise the RTC stops.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-18 6:18 AM
Solved this, but didn't really understand how. I enabled the BYPSHAD bit in the RTC CR to access the registers directly, not through the shadow registers and it started working. I think the shadow registers were not being updated, but somehow watching the registers in the debug mode, made those registers being updated. If someone really understands how this works, please post here.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-18 6:21 AM
And when you connect with the debugger to a board which previously run without the debugger (i.e. ''clock not running''), what is the time?
JW- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-01-18 6:26 AM
> If someone really understands how this works, please post here.
It's described in details in RM0090 rev.11, ch.26.3.6. JW