Skip to main content
sheinv
Associate
January 19, 2016
Question

Troubles with TIM1 PWM generation via DMA.

  • January 19, 2016
  • 0 replies
  • 416 views
Posted on January 19, 2016 at 15:59

Hello. I have some troubles when implementing PWM generation on the timer TIM1. I use STM32 HAL Library. I have to update the values of registers CC1�CC3 each time when TIM_UPDATE event happens. I planned to use 2 memory chunk for it. When the first one is used as a ''warehouse'' of the values that DMA will provide to TIM1 CC1�CC3 values, I'll use the second to fill it up with the new values. I think to implement this with DMA. I tried to do it through the function HAL_TIM_PWM_Start_DMA but without success. This function can be only called for a single channel but I need to enable generation on 3 channels simultaneously. Sequential calls to HAL_TIM_PWM_Start_DMA for any another channel returns HAL_BUSY. Besides of that I tried to use the function HAL_TIM_DMABurst_WriteStart but also without success. I need to transfer much more 18�4 words.

Ok, I solved my problem. Thanks! :)

#tim-pwm-dma-stm32
This topic has been closed for replies.