STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST virtual com port issue in case of MCU reset

Posted on February 22, 2014 at 17:03I have a problem with serial-over-USB port reconnection after stm32f4discovery board reset (for instance, re-programming) - with the native USB controller port, not the uart dongles. I have originally reported thi...

arro239 by Senior
  • 6403 Views
  • 14 replies
  • 0 kudos

How to generate a DC level on STM32F4 DAC?

Posted on August 30, 2016 at 03:56Hi, I am using pin PA4 as a DAC output on an STM32F405. I then have a unity gain op-amp buffer. My supply is 3.3V. What I want to do is rather than create a SINE output at some frequency, is to generate a DC signal....

NUCLEO-L152RE + FatFs + uSD + SPI

Posted on August 29, 2016 at 12:22Hi, I have bought me a Nucleo-L152RE board to test the STM32L152 MCU. Now I want to write data to a uSD card using the FatFs file system. Since this STM32 MCU doesn't have a SDIO bus, I want to use SPI. Does anyone ...

lrsolem by Associate
  • 1233 Views
  • 1 replies
  • 0 kudos

I2C repeated START

Posted on February 27, 2016 at 10:53 Hello I am using STM32F030CC to communicate with BQ3060 fuel gauge through SMBus. Everything is working kinda fine, but I am little worried about my repeated start condition. I know reading 2 bytes ...

0690X00000605MVQAY.png
karlis by Associate II
  • 4855 Views
  • 5 replies
  • 0 kudos

Suggestion for TIM_DMABurst_WriteStart()

Posted on August 04, 2016 at 12:07   Dear, I want to generate the 4 signals for a H bridge to create a sinusoidal signal by pwm So I used Timer 1 and its 4 channels powered by a DMA in burst mode The PWM data are organized in an array of 360 structu...

WWDG

Posted on July 17, 2015 at 16:18Hi,I am having problems to run the WWDG in a STM32F405.I am using the HAL Drivers from Cube MX.The process is the following:{__HAL_RCC_WWDG_CLK_ENABLE();MX_WWDG_Init();HAL_WWDG_Start(&hwwdg);HAL_WWDG_Refresh(&hwwdg,12...

lucas23 by Associate II
  • 2618 Views
  • 5 replies
  • 0 kudos

interrupt in overflow event of timer in up/down mode

Posted on August 02, 2016 at 10:58Hello,I use a nucleo stm32f401RC Evaluation Board for the regulation of a boost converter and I need to generate the interruption on the ON half-signal of PWM and I need also synchronize the conversion of 3 channel ...