User Activity

Posted on November 30, 2017 at 09:59Hi,I have some issue setting up CAN for STM32F302 using Keil. As a starting point I used the Keil STM32 CAN Example:http://www.keil.com/download/docs/351.aspEverything seems to work, except the interrupt handling....
Posted on November 23, 2017 at 17:17Hi,I�m having some issues getting a dual FS USB Host RTOS configuration running based on a STM32F746 target.Connection events and callbacks events work correctly.When I use the USBH_Init() function for initialisin...
Posted on October 28, 2017 at 14:31Hi,which user AC6 project can be used in combination with STEVAL_IHM042V1?I would like to use the STEVAL_IHM042V1 to run two motors with hall sensorsIs it: \Web\Project\AC6\STM32F30x_UserProject -> config STM32303C...
Posted on October 12, 2017 at 21:54Hi,Running the configuration below:-NUCLEO-F302R8-X-NUCLEO-IHM07M1-FOC SDK 4.3Succesfully tuned BLDC motor with the Motor Profiler. Also in Play Mode the motor runs very well.Next step is running the BLDC motor usi...
Posted on October 09, 2017 at 08:04We are trying to setup a small BLDC motor with the Motor Profiler utility.-X-NUCLEO-IHM07M1-FOC SDK 4.3-Custom motor: 2 pole pair BLDC 18VDC, 2W @ no load, 4000 rpmWith this setup the Motor Profiler is not able to ...