STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

*** Command Line Programmer for STM32F107

Posted on May 19, 2016 at 16:47I used to work with http://www.ti.com/product/MSP430F47197 and I found out that there is a Flasher which gives you this ability to load the code through a batch file. So, I am just wondering if you guys are familiar wi...

I²C Level Shifting Required for STM32L4?

Posted on August 10, 2016 at 10:00I operate an STM32L4 at 1.8 V and I�C peripherals at (up to) 3.6 V. The data sheet (DocID028794 Rev 2, table 21) is pretty clear when it comes to FT_xx inputs. But when it comes to FT_xx outputs I trip over the foll...

STM32 USB CDC on MAC OSX

Posted on August 31, 2016 at 15:00Any one has experience of developing STM32 USB CDC applications on MAC OSX? Is there a driver for STM32 USB CDC on MAC OSX? I have a HW working well on Windows with VCP driver 1.4.0, however, this HW is recognized a...

frank23 by Associate II
  • 752 Views
  • 0 replies
  • 0 kudos

Need Working Code for STM32F107

Posted on August 30, 2016 at 19:15Here i enclosed the Working Code For STM32F103.i Want to Convert this code to STM32F107 for Project Needs. This Code Not work in STM32F107 25Mhz Board .How can i init SPI According to the Board. This code Interface ...

senthil by Associate II
  • 1199 Views
  • 2 replies
  • 0 kudos

Audio streaming clock sync

Posted on February 13, 2013 at 17:00I am interested in techniques for synchronizing the STMF4 I2S clock with an incoming audio stream on the USB. The clock on the source and the clock on the STM32 board will always be slightly out of sync causing ei...

ajgboomer by Associate III
  • 14600 Views
  • 33 replies
  • 0 kudos

CAN filters

Posted on May 11, 2012 at 08:03Hello everyone! Can anybody help me to understand the following thing about filters in CAN for stm32f10x. 1) Can I configure filters for receiving only messages with the specific range of ID values. For example, I want...

STM32F767ZI Hard fault when using ITCM RAM

Posted on August 30, 2016 at 19:05I am playing with the ITCM RAM on a Nucleo-144 board. I am having problems with the ITCM RAM causing a hard fault when I call a subroutine from inside a subroutine. I have successfully used the ITCM RAM to store a f...

STM32F100RBT6B l293d 28byj-48

Posted on August 29, 2016 at 13:08 Hello i am trying to launch simple stepper ( http://robocraft.ru/files/datasheet/28BYJ-pdf) using l293d. Connecting 28byj-48 to the L293D: Engine contact 1 is connected to the output 1. E...

anton23 by Associate II
  • 1036 Views
  • 1 replies
  • 0 kudos

SDADC and ADC Calibration Time Interval

Posted on August 29, 2016 at 22:44If a processor is to be run continuously for weeks, months, even a year or more is it sufficient to calibrate the SDADC and ADC once at power up, or would there be a benefit to calibrating at regular time intervals?...

spflanze by Associate II
  • 2075 Views
  • 2 replies
  • 0 kudos