STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Mouse and Keyboard USB HID stm32f042

Posted on September 26, 2016 at 18:14In separate applications I have managed to control the mouse, and the keyboard using the stm32f042. How do I go about combining the two in one application?I would like my stm32 to be treated as both a keyboard an...

STM32F769I - Possible CAN errata

Posted on September 20, 2016 at 20:29 During evaluation of this chip, we found thatthe microcontroller apparently sets the ACK bittoo early when receiving messages from other devices. Bus was 250 KBaud with a sample point of 80% (also tried 75% a...

holeman by Associate II
  • 2332 Views
  • 5 replies
  • 0 kudos

SPI Slave Tx DMA wont stop

Posted on September 26, 2016 at 09:12 In my application STM32F411 is a SPI slave (TI mode) and the master microcontroller transmits data as packets perpetually till an acknowledgement is received from STM After a packet of data is received by ST...

siva by Associate
  • 953 Views
  • 1 replies
  • 0 kudos

RTX Configuration via STM32CubeMX

Posted on September 26, 2016 at 11:56Hi,I would like to use CubeMX and its grafical interface to generate code for my project in the Keil uvision IDE. I would like to use RTX RTOS too.I only found this tutorial:http://www.keil.com/pack/doc/STM32Cube...

jbeloso by Associate
  • 2408 Views
  • 2 replies
  • 0 kudos

STM32 Discovery Board vs Evaluation board

Posted on September 23, 2016 at 12:39Hey guys,I'm thinking of buying a discovery board or evaluation board. However I'm not sure which one to choose.I'm currently working on an Arduino for a private project, but arduino has 2 Major disadvantages: 1)...

ETH DMA stuck in ''waiting for status''

Posted on September 21, 2016 at 15:36Hello. I'm working on a project, running on STM32F427IIH6, which uses FreeRTOS 6.1 and LwIP 2.0. There are several TCP clients and TCP/UDP servers and it's running with no issues. But after adding UDP client, lo...

danicek by Associate
  • 1598 Views
  • 2 replies
  • 0 kudos