cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube migration issue

nbobovnikov
Associate II
Posted on March 19, 2016 at 14:59

Hello!

After regenerating the project created from previous version of the CubeMX, using new version (4.1), some user defined code has been lost in stm32f1xx_it.c file (image with diff is attached)

Best regards,

Nikolay Bobovnikov

!stm32-!cubemx-!bug

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Nesrine M_O
Lead II
Posted on March 21, 2016 at 14:06

Hi Nikolay Bobovnikov,

Thank you for your feedback. The issue has been reported internally.

-Syrine-
stm32cube-t
ST Employee
Posted on March 22, 2016 at 14:58

Dear user,

Can you please provide the following additional information:

Which MCU you  had selected.

With which MX version  the project was initially done (4.12, 4.13, earlier)

Which option did you  choose when loading your project in 4.13.1: migrate or continue?

Can you also attached the .ioc configuration file of your project.

Thank you

nbobovnikov
Associate II
Posted on March 23, 2016 at 17:44

Hello,

I'm sorry, now I'm not sure about exact version of CubeMX, it was probably 4.11 (definetely not earlierd). I use this MCU: STM32F103C8T6. I chose ''migration'' after installing new version of CubeMX. Project file is attached.

________________

Attachments :

stm32f103c8t6.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Htp5&d=%2Fa%2F0X0000000aXI%2F654flIbi8mJxeibAgDIcY2GZ8Y86aIdlwUDvVvKPABA&asPdf=false
stm32cube-t
ST Employee
Posted on April 19, 2016 at 10:52

Dear user,

Sorry for the inconvenience.

The generated file stm32xxx_it.c has been enhanced and may have broken compatibility with previous version. That's why it is recommended to back up your project prior to a migration.

On top, it looks like a bug has been fixed in latest version: On your selection you can no longer accommodate both I2C1 in I2C mode and Timer3 with TI1FP1 trigger source.

Best regards