STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Possible bug in HAL USART Driver

Posted on September 11, 2016 at 16:41I am experimenting with FreeRTOS and the HAL layer using an STM32F4 DISCO board.I have two threads.  One reads from the serial port and send the byte read, in a message to a second task.The second task, blocking ...

STM32L476 I2C speed setting accurately?

Posted on September 24, 2016 at 01:37Hi there,I got an issue recently when I was trying to set up the I2C speeds for STM32L476RG. I can set it up for an approximate value but never get the exact one. For example, I want to achieve 100 kHz while I ca...

jiayuan by Associate II
  • 3491 Views
  • 2 replies
  • 0 kudos

What SWD/ISP/JTAG to use with STM32F407?

Posted on September 24, 2016 at 00:16I am building a testboard with a 100pin 407VGT in it. There is no room for USB on it. After reading the HW manual I still don't know what is a correct/best programmer connector to use. There are 6 pins in Discove...

LMI2 by Lead
  • 3539 Views
  • 4 replies
  • 0 kudos

stm32L476RG nucleo dev board

Posted on September 23, 2016 at 20:00I am losing my mind, I start cubemx, installed stm32L4 library, configure the clock HSI , as this board has no HSE, GPIO and SPI, choosed MDK 5,  I generate the code, and try to test GPIO using Hal api, nothing h...

Declaring variables in External SRAM

Posted on September 23, 2016 at 18:33Hi everyone!  I'm having some difficulty getting variables to be declared in external SRAM.  I'm using a STM32L4.  If I do address casting like the FMC example project for the eval board in the library code I can...

Jim Kaz by Associate II
  • 1998 Views
  • 1 replies
  • 0 kudos

Program received signal SIGINT, Interrupt

Posted on September 23, 2016 at 11:06Hi, I am using STM32469I-Evaluation board (384KB SRAM and 2MB flash), Cube MX version 4.16, SW4STM and AC6 tool chain version 1.8v (32bit OS) and ST-Link V2.1 debugger (firmware version V2.J27.M15). I have create...

One-Wire protocol with Input capture

Posted on September 23, 2016 at 12:07Hi to all i have this problem, i have a STM32L152RE with a temperature Sensor, this sensor use 1-wire protocol,the data is codifing with pulse width, lather the mcu start the connection the sensor give the 40 bit...

antonioB by Associate II
  • 827 Views
  • 1 replies
  • 0 kudos

STM32F756NG and ADC conversion time

Posted on September 23, 2016 at 12:26APB2 clock: 100Mhz ADC clock: 100/4=25Mhz Data resolution: 12bit One conversion time = 15/25 = 0.6us, 6 conversion is 3.6us But in real environment when i test on device i got the result: 6 conversations = 1.8us ...

ctbk1989 by Associate
  • 549 Views
  • 0 replies
  • 0 kudos

STM32F407G-DISC1 - RTC - HAL

Posted on September 22, 2016 at 09:39hi guys   im currently working on the STM32407G-DISC1, the goal is RTC usage. HWlib is HAL. Below i posted the RTC related code. I did check both the CubeMX autogenerated code as well as the F4 RTC example as we...