STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0B1RE Using a timer to sample a clock signal

Hello and thank you for taking the time to read and answer my question. What I want to do:I have SYSCLK configured at a frequency of 16 MHz (using HSI), and a PLL block clock with a frequency of 18 MHz.I want to sample the PLL clock on the rising edg...

undacmic by Associate III
  • 4802 Views
  • 13 replies
  • 7 kudos

Resolved! RTC wake up time counter limit

In my app, I need MCU to go to stop mode and then wake up by RTC timer. I follow this RTC wake up example and manage to make MCU go to stop mode for a few seconds and then wake up. Because in my app, we want MCU to wake up once in a few hours instead...

HDaji.1 by Senior
  • 5131 Views
  • 5 replies
  • 2 kudos

Resolved! stm32L496 error clock offset

Good morning community,I am using the STM32L496QGI6 for a certain application using the uart to send and receive messages, in this case it always gives me symbols even with the baudrate correctly configured, I have checked the clock configuration and...

CamiloRJ9_4-1737385379622.png CamiloRJ9_0-1737385338471.png
CamiloRJ9 by Associate II
  • 1957 Views
  • 4 replies
  • 3 kudos

Resolved! Documentation on CAN bus

Can anyone give a hint on where to look for proper documentation on CAN bus development? I see some primitive examples online, though there are a lot of moments that are not explained as they shouldFor example, CAN filtering and identificator masking...

Siemens by Associate
  • 3058 Views
  • 6 replies
  • 6 kudos

Resolved! STM32 Maximium Pin Voltage in Output Mode

Hello,we use the STM32G474 with a single supply voltage of 3V3 at the VDD Pins.At the moment we investigate defective microcontrollers. The Microcontrollers are defective after several hours with the 3V3 VDD voltage supplied. The defective is an incr...

5VTolerant.PNG