STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Input resistance of analog input, reset (?)

Dear community, my Nucleo H723ZG captures analog signals via channels (see attachment) :ADC12_INP15,ADC12_INP10 andADC12_INP10 The second one reads a 4-20mA pressure signal from a sensor with the help of an external shunt resistor. After a system res...

LysAn by Associate III
  • 1333 Views
  • 1 replies
  • 1 kudos

BootLoader timeout

Posted on January 12, 2015 at 09:17HiI am using STM32L151 bootloader.I wanted to run the bootloader at program start, and if no usb if attached for a certain timego back to regular application.Is it possible to configure a timeout for the bootloader...

yarona by Associate II
  • 2312 Views
  • 4 replies
  • 3 kudos

stm32h7 dual core debugging

Hi all. I am using STM32H747BIT6 with cm4 & cm7 cores but I am struggling with debugging my application. I started a new STM32 project using the CubeIDE wizard and gave the ioc file to generate simple code. Then I built the two projects (m4 & m7). Af...

yonatan by Associate III
  • 1932 Views
  • 2 replies
  • 0 kudos

Resolved! stm32g0b0ce flash page erase issue

Hello folks I am using the first bank for the firmware and the second bank to save a bunch of parameters. When the fw receives a command via uart, it updates the parameters erasing first and then writing groups of 8 bytes. When I try to erase the fir...

max65 by Associate II
  • 1960 Views
  • 3 replies
  • 0 kudos

Nested interrupts on the Nucleo-F411RE

 I am doing an academic activity where I was asked to execute a reading process from an external RTC via i2C, but on another MCU, I used a repeat timer, but I was unsuccessful. Something seems to interfere with the I2C communication and according to ...

STM32F373C8T6 Foot print and Symbol wrong Pinouts

I down load the STM32F373C8T6 Foot print and Symbol from STs website (Ultalibrarian)But it has a wrong Pinouts connections (Pin numbers) VDD_2    Pin No.14PA-4       Pin No 15PA-5       Pin No 16PA-6       Pin No 17 But actual connections arePA-4.   ...

vbakoti by Associate
  • 881 Views
  • 1 replies
  • 1 kudos