STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 Maximium Pin Voltage in Output Mode

Hello,we use the STM32G474 with a single supply voltage of 3V3 at the VDD Pins.At the moment we investigate defective microcontrollers. The Microcontrollers are defective after several hours with the 3V3 VDD voltage supplied. The defective is an incr...

5VTolerant.PNG

QSPI reads only 0x9999

I have a custom board with STM32H747IGT6 MCU, which communicates with a S25HL512TFAMHI010 flash memory chip over QSPI. I have made several iterations of this board, and the QSPI communication has always been fine.However, on the most recent iteration...

Resolved! QSPI RAM on OSPI Interface of H7A3 MCU issues

Hi Guys,I need some help / input:I am trying to get the communication running between my Nucleo H7A3 and a Shield with a ISSI QuadSPI RAM in a SOP-8 Package running.Scenario:I am debugging with my Scope, I have a digital Probe on all 6 lines (CSn, Cl...

CBerg by Senior II
  • 2946 Views
  • 7 replies
  • 0 kudos

Problem setting up UART on STM32F756VGH6

Hi,I am learning and exploring the STM32F756VGH6. My goal is to setup a simple UART and send some data to the PC using USB-UART serial converter and  puTTy terminal on PC. I am using register based coding approach as it makes the code more efficient....

Vilius by Associate III
  • 4049 Views
  • 10 replies
  • 5 kudos

Resolved! USB XACT_ERROR response on BulkIn request

Hi all,we are developing a board based on STM32F429 chip.In particular I'm developing a composite USB device on USB OTG port, showing a custom device + a CDC device [ep 0x85, 0x06, 0x83] using USB_Device_Library code.Windows correctly shows 3 items: ...

SteMMo_0-1734001551484.png
SteMMo by Senior
  • 2207 Views
  • 3 replies
  • 0 kudos