STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F373C8T6 Foot print and Symbol wrong Pinouts

I down load the STM32F373C8T6 Foot print and Symbol from STs website (Ultalibrarian)But it has a wrong Pinouts connections (Pin numbers) VDD_2    Pin No.14PA-4       Pin No 15PA-5       Pin No 16PA-6       Pin No 17 But actual connections arePA-4.   ...

vbakoti by Associate
  • 858 Views
  • 1 replies
  • 1 kudos

STM32G0B1RE Using a timer to sample a clock signal

Hello and thank you for taking the time to read and answer my question. What I want to do:I have SYSCLK configured at a frequency of 16 MHz (using HSI), and a PLL block clock with a frequency of 18 MHz.I want to sample the PLL clock on the rising edg...

undacmic by Associate III
  • 4717 Views
  • 13 replies
  • 7 kudos

Resolved! RTC wake up time counter limit

In my app, I need MCU to go to stop mode and then wake up by RTC timer. I follow this RTC wake up example and manage to make MCU go to stop mode for a few seconds and then wake up. Because in my app, we want MCU to wake up once in a few hours instead...

HDaji.1 by Senior
  • 5039 Views
  • 5 replies
  • 2 kudos

Resolved! stm32L496 error clock offset

Good morning community,I am using the STM32L496QGI6 for a certain application using the uart to send and receive messages, in this case it always gives me symbols even with the baudrate correctly configured, I have checked the clock configuration and...

CamiloRJ9_4-1737385379622.png CamiloRJ9_0-1737385338471.png
CamiloRJ9 by Associate II
  • 1911 Views
  • 4 replies
  • 3 kudos

Resolved! Documentation on CAN bus

Can anyone give a hint on where to look for proper documentation on CAN bus development? I see some primitive examples online, though there are a lot of moments that are not explained as they shouldFor example, CAN filtering and identificator masking...

Siemens by Associate
  • 2999 Views
  • 6 replies
  • 6 kudos