STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030K6T6 support touch library?

Posted on December 12, 2016 at 12:00hiin this doc en.DM00210526.pdf there is no name of STM32F030K6T6 to know which pin is which Chanel of touch.and in STM32F030K6T6.pdf there is no name of touch in pin configuration.can i use touch library on this ...

How to Turn off all clock of STM32L0xx ?

Posted on December 12, 2016 at 14:43Hello,I am using STM32L0xx MCU in stop mode. but can able to achieve low power as given in datasheet?Please help me to turn off clock and also i want suggestion to achieve it.Thank you in advance. #turn-off-all-cl...

RTC Misbehavior and strange display

Posted on December 13, 2016 at 15:36Hi, I'm working with STM32L486RG ultra low power microcontroller using the IAR v7.4 IDE.I'm using the RTC peripheral in order to get the real time clock . My clock source is an LSE crystal which has 32768Hz as fre...

0690X00000603HzQAI.jpg 0690X00000603VGQAY.jpg 0690X00000603VBQAY.jpg 0690X00000603L0QAI.jpg

I2C Timeout waiting for TXIS flag

Posted on December 12, 2016 at 17:26ST Community,I have been trying to get I2C communication working on my STM32L073RZ Nucleo board for some time now, but to no avail. After doing a bit of stepping through the code, it looks as though a HAL_TIMEOUT ...

conner by Associate II
  • 6990 Views
  • 2 replies
  • 2 kudos

STM32F207 Nucleo 144 Board UART2 Data Receiving

Posted on December 09, 2016 at 14:19Hello,I am using STM Cube MX for designing the UART2 Communication over STM32F207 Nucleo 144 Board. I have designed the Code for tranmitter part & it worked fine. I am getting data on PC (Tera Term Interface).Now ...

Resolved! ADC circuit

Posted on December 09, 2016 at 20:51Hello, I am working on a design on stm32f407vgt6 which I don't want to use the ADC & DAC so I don't have to connect the circuit of ADC and leave VDDA&VSSA&VREF floating?#clive1

BLDC faults using Motor Control Library (FOC SDK v4.2)

Posted on October 11, 2016 at 11:31Hello everybody, I am trying to run a BLDC motor with the FOC SDK v4.2, using a STEVAL-IHM021V2 power stage and STMF32F303RE Nucleo board as MCU. I set everything up with no trouble and connect the board to MC Wor...