User Activity

Posted on July 18, 2016 at 20:01The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on July 11, 2016 at 09:53Why does Nucleo 64 not have the sound ouput module I2S DAC as extenstion board?Nucleo 64 is really comfortable for audio eval project. Why didn't ST add the I2S extension eval board?ST added some code for I2S DAC but ...
Posted on June 16, 2016 at 11:36Hello. In a very specific project I have to use 2 different I2S codecs one for input and another for output. Is it possible to do it in 1 project on same CPU? The frequencies are different. And the Data type is seems ...
Posted on June 11, 2016 at 20:44I use the DFSDM in multichannel sound card USB. It is 1st time for me.I have read that the average DFSDM has 8 channels.When I started the project I have found that STM engineers added only 4 filters for 8 channels. I...