STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411 firmware download issue in DFU mode

Hi Everybody,     I am facing a wired issue in programming the  mcu . I have designed  a custom borad with STM32F411CEU6 (QFN-48 package). DFU mode is is properly detected.  But whenever I am trying to connect the mcu  with STM cube programmer in dfu...

STM32F103C8T6 Program not working and USB not recognized

Hello,I found this schematic and layout with a stm32f103c8t6. I ordered it and wanted to programm it.With stm32cubeprogrammer I detect the stm32 no problem via ST-LINK.Same with stm32cubeide I can download successfully the code.But now the problem is...

Basic_STM32_Bluepill.png pcb.PNG stm32cubeprog.PNG code.PNG
JTAPIE by Associate II
  • 7067 Views
  • 17 replies
  • 3 kudos

Resolved! HAL_Delay problem when adding ThreadX to the project

Hello everyone,I'm working on the µc STM32H5, I have an application that runs correctly, and when I configure the threadX in the project for which I've configured the TIM6 as the basic timer and I've released the SysTic for the threadX using CubeMx. ...

wMESTIRI by Associate II
  • 2305 Views
  • 5 replies
  • 2 kudos

stm32wle5ccu6 stopmode disables programming

Edited to apply source code formatting - see: How to insert source codei am new to the programming and i am working on a stm32wle5ccu6  board and accidently flashed below firmware. later the PORT is not detecting and not able to reflash the device. (...

Resolved! STM32U5A9 boot fail at low temperatures

Hi,We have a design that at normal temperatures runs fine (21C). If it goes below 0C it starts failing to boot.The system has the Secure Boot Secure Firmware Update (SBSFU) system on it. We found that putting a delay at the start of the main() functi...

NPato by Associate III
  • 5055 Views
  • 14 replies
  • 11 kudos

stm32f103c8t6 usb driver for windows 10

Posted on November 14, 2016 at 13:04hello this is my first try to work with ARM and I bought stm32f103c8t6 that is simple to start with it a few days before i buy a big development boardI have a problem in installing usb driver on windows 10 for stm...