STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411/RM0383 bad GPIOA->MODER reset value

Posted on January 31, 2017 at 16:57Hello,page 153 tells:8.4.1 GPIO port mode register (GPIOx_MODER) (x = A..E and H) Address offset: 0x00 Reset values: · 0x0C00 0000 for port AThis does not make sense and a look at a real device after reset gives:(...

Resolved! STM32F7 bootloader usart comm

Posted on January 31, 2017 at 15:56Hi All,I'm working with a board with two STM32F7 processors and trying to connector to the built in bootloader on one from the other via USART. The TX/RX lines are connected to the target on USART3 and on the maste...

hbarta2 by Associate III
  • 1975 Views
  • 2 replies
  • 0 kudos

WKUP and EXTI

Posted on January 31, 2017 at 15:52Hello!I have a basic question about the association between WKUP and EXTI signals in a STM32. I am using a STM32L467.My system has a push button that I want to use to wake the mcu from the STANDBY power mode. I als...

TIM1 Break Interrupt

Posted on January 31, 2017 at 16:06I have an Active Low signal for break. But the Interrupt seems to be Active High Level sensitive.Doesn't the interrupt TIM1_BRK_IRQHandler respect TIM_BDTR_BKP (polarity)?Chip: STM32F103

Jeroen3 by Senior
  • 915 Views
  • 0 replies
  • 0 kudos

Resolved! EWUPx and Stm32F412

Posted on January 31, 2017 at 13:49Hello,while DocID027813 Rev 4 chapter 5.4.2 knows aboit EWUP1..3, e.g.* @file stm32f412zx.h * @author MCD Application Team * @version V2.6.0only knows EWUP.EWUPx should be added in other headers too, where applicab...

stm32L476 12 Bit ADCs causing Spikes in Data

Posted on January 30, 2017 at 19:29Hi there,I am using the Stm 32L476 and I am trying to use 2 ADCs with 2 channels each with 12 Bit. So 4 Channels all together. I am using the ADCs in Regular simultanuous  multimode with DMA so I am able to transmi...

Bene Sch by Associate II
  • 3559 Views
  • 7 replies
  • 0 kudos

TIM3 Clock Frequence is ZERO

Posted on January 31, 2017 at 10:02Hi, everyone! I am writing code for a NucleoF303K8,using std periph lib . I am trying to output PWM via the D3 pin, which is PB0 of the chip. It doesn't work. So I try to find out what's wrong. But when checking th...

Li JW by Associate II
  • 2157 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F427 DFU-Mode

Posted on January 31, 2017 at 08:21Hello,I try to implement a bootloader via dfu mode.In my applicationi write a magic value and perform a reset.In the bootlaoder i read the magic value and try to jump to the system memory.Therefore i try this:Bootl...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.