2016-07-05 3:47 PM
Hello,
I am trying to read the data0/data1 fields from the flash option byte register.When the flash read protection level is 0 - I can do that no problem, but when the read protection is set to 1 it fails.According to the reference manual there should be no problem to read the option bytes under protection level 1.Any help is highly appreciatedThanks,ron #option-bytes #flash #stm32f32016-07-05 4:30 PM
Read it from where, and with what?
Code in the F3 should be able read and display the state of the option bytes whatever the protection level externally.2016-09-02 4:21 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.