STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the 'Debug Serial Wire' ?

Posted on March 29, 2017 at 13:02Hi  I am testing the ADC on the STM32L0 chip, and using the STM32Cube. The demonstration I have ticks the 'Debug Serial Wire' in the SYS folder. It is not explained to what this is, can anyone let me know what this a...

Injected ADC convesion problem

Posted on March 29, 2017 at 21:00This is screenshot from ST FOC User Manual. Here is injected one ADC conversion, triggered by TIM1_CH4. I need add injected conversion on timer update event (red point - fixed, green - isn't). Is it possible?I alredy...

0690X00000606ZMQAY.png
signx by Associate II
  • 811 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F030R8T6 TIM1 PWM NO WORK FOR STM32CUBEMX

Posted on March 27, 2017 at 19:20 HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_3); HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_1); HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_2); HAL_TIM_PWM_Start(&htim1,TIM_CHANNEL_4); __HAL_TIM_SET_COMPARE(&htim1,TIM_...

JACK TAN by Associate II
  • 2464 Views
  • 6 replies
  • 0 kudos

STM324x9I_EVAL and external Flash

Posted on March 29, 2017 at 14:23Hellorecenty I bought an STM324x9I_EVAL and I would try to run the STemWin_SampleDemo in the external flash. My toolchain is MDK_ARM an I use Keil 5As I know, I need Add a Programming Algorithm for the external flas...

Nickjmas by Associate III
  • 846 Views
  • 1 replies
  • 0 kudos

Difference with DMA between F746ZG and F746IG

Posted on March 28, 2017 at 15:34Hi, before receving my new board, I develop application on NUCLEO-F746ZG (at 25 MHz). I use a DMA on RX of USART3 (DMA1 Stream 1 Channel 4). All works fine. When I received new board with STM32F746IG (at 8 MHz), the ...

stm32F769I-Disco with FreeRTOS as MSC USB Host

Posted on March 28, 2017 at 12:58Hello,i am trying to read/write to an USB-Stick thru the HS USB-Port,i setted up CubeMX with FREERTOS, USB_HOST HSIP Mass Storage Host Class, enabled FATFS on USB-Disk  and set USB_OTG_HS external Phy Host_Only (besi...

Read/write cycle life of RTC backup registers (STM32F373)

Posted on March 28, 2017 at 09:54Hi all,I'am using STM32F373 MCU, in my application, the RTC backup registers updated every 10 minutes.I know some memory cycles limit read/write cycles, Eg, Eeprom memory only allows 10000 write /read  cycles, if gre...

Please add DBGMCU_IDCODE value in system headers

Posted on March 28, 2017 at 19:51Hello,the system headers now define many bit positions in the DBGMCU_IDCODE register. However they don't define the actual value for the device. Please, add the actual value if the IDCODE in the headers, so that code...