STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to programme a powerstep01?

Posted on April 25, 2017 at 10:09Anybody who can teach me how to use a powerstep01 to drive the step motor?I have the demo boards and the powerstep01 works well with the demos and the download software from st.com.Now, i want to use another MCU (low...

Lin SS by Associate
  • 1059 Views
  • 1 replies
  • 0 kudos

Resolved! I need help

Posted on April 26, 2017 at 10:44Hi,I am newbie in System Workshop for STM32. I tried write simple example - LED blink. It works fine.Now I want to test the same program, but with a timer interrupt.In file ''stm32f4xx_hal_conf.h''  I enable HAL_TIM_...

0690X00000602S7QAI.bmp 0690X00000602SLQAY.bmp 0690X00000602SaQAI.bmp
Peko by Associate III
  • 1503 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo L432KC bootloader via UART failed

Posted on April 25, 2017 at 10:23Hi, I met a problem using bootloader on pc to wirte program into STM32L432KC via UART.Here is the process I did :1,I connect D1/Tx and D0/RX(PA9 and PA10 of STM32L432KC) to CH340 USB to UART board, 5V Vin and GND. US...

0690X00000605tnQAA.png 0690X00000605w5QAA.png 0690X00000606r0QAA.png
Yu LU by Associate II
  • 2813 Views
  • 4 replies
  • 0 kudos

RTL 000.0 TCP-ERR:Send, Socket 1 reentrant callback

Posted on April 26, 2017 at 09:44hi,I  work on rtl-tcp over ppp protocol. First gsm modüle is given IP by AT commands and then is connected ethernet over ppp protocol.  At software , tcp socket is opened and tcp_send function is worked over ppp . RT...

ali2399 by Associate II
  • 709 Views
  • 0 replies
  • 0 kudos

Change uart baudrate on the fly

Posted on March 22, 2017 at 11:45Hi everyone,i just would like to know know the sequence of reintializing UART port to a new baudarte or change parity on the go during execution.  I am using Hal library. What would be the sequence to do so and does ...

Raider E by Associate III
  • 6450 Views
  • 10 replies
  • 1 kudos

STM32F103RET6 PWM

Posted on April 25, 2017 at 19:49Dear Sir .I am configuring A8,A9,A10,A11 for PWM OUTPUT.I don't get an pwm output on PA9 , If I configure PA9 as output , Than I can toggle it.Attached some code/* Configure PWM Outputs */ GPIO_InitStructure.GPIO_Pin...

Problem with USBHS and FATFS - STM32F407

Posted on April 26, 2017 at 02:46I'm using STM32f407 with USB 3300 ULPI module, and try to copy file from SD card using SDIO to flash memory using fatfs. The drive mounted and file opened successfully, but while reading or writing data on flash memo...

Resolved! X-NUCLEO_CCA02M1

Posted on March 19, 2017 at 12:38Hello all,I have bought a NUCLEO-L476RG board and a X-NUCELO_CCA02M1 board a couple of months ago and I have flashed the stm32f476RG micro of the board with the sample application that it is include in the folder...\...

0690X00000606bCQAQ.png