cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX Feature Request

valtin
Associate II
Posted on November 29, 2016 at 22:26

Hello,

I like CubeMX and would like to suggest a feature for the report generator.

I use Nucleo boards a lot for development and small projects and the support for it is really great, but I always have to look up the layout of the Nucleo headers.

I usually end up on mbed.org like for the F401:

https://developer.mbed.org/platforms/ST-Nucleo-F401RE/

And I was wondering if that would not be a great thing to have in the report generated by CubeMX, alongside the pin layout already there.

I would suggest a layout similar to the mbed website with all the available ports + special functions, and also a extra column for the own pin label.

Because the basic layout is the same for the Nucleo32/64/... a general image with some custom rendered text should do the trick.

Maybe the information (like pin mapping) is also already available in CubeMX. The name/type of the Nucleo Board at least is already there.

I am looking forward hearing from you.

Sincerely Markus

#feature-request
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on November 30, 2016 at 08:35

Dear User,

Your request is reported internally to our CubeMx team.

Thank you for fast feedback and for your contribution in the STM32 Community.

All comments and suggestions are welcome to improve our solutions.

Best Regards

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen